unknown error with key professionaleditionMCU 10.3, LM_NOTTHISHOST

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unknown error with key professionaleditionMCU 10.3, LM_NOTTHISHOST

2,473 Views
rossrhone
Contributor III

Trying to licence my CodeWarrior  MCU 10.4 with a usb dongle, but continue to receive this unknown error message. Anyone else had this error and was able to fix it?

 

Thanks!

Labels (1)
0 Kudos
Reply
2 Replies

2,316 Views
TomasPaez
NXP Employee
NXP Employee

LM_NOTHISHOST DOnGLE

This error The hostid of this system does not match the hostid specified in the license file. Make sure dongle Id match with the license file host. 

Error might be a problem with the Dongle detection or match, is either not connected or not being recognized by the system.

I suggest to try the license file using as host ID the disk serial number or Ethernet MAC address instead of dongle device. 

0 Kudos
Reply

2,316 Views
rossrhone
Contributor III

Is the dongle ID also referred to as the FLEXID in the System Settings of the program LMTOOLS "Flexera Software"? If so the FLEXID number in that software is different the the number provided to me in my license file. I am also using the configuration settings in the "Service/License File" tab in LMTOOLS. I have manually edited the FLEXID number in the license file to match my dongle's FLEXID number and it spits out an error message of "Error with key Professional... ,license key in license file does not match other data in file." 

Thanks,

Ross

0 Kudos
Reply