how to register codewarrior V3.2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to register codewarrior V3.2?

跳至解决方案
2,584 次查看
kyleden
Contributor I

V3.2 , error"the codewarrior ide is licensed and a valid license key was not found "...feature:win32_cwide_limited.

标签 (1)
0 项奖励
回复
1 解答
2,348 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

I've installed CW for M68K v3.2 on  Win 7 64 bit OS and with the professional suite license, I can use the tool without problem.

What is the license file used ?

For this tool version, only the Professional Suite is available.

Attached you will find a temp license file.

This license file will expire the 15-nov-2015.

Rename the attached file to license.dat.

Have a great day,

Pascal

Freescale Technical Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,348 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

To investigate the problem, we need to know exactly the CodeWarrior version you're using.

To do that you must:

  Under CodeWarrior IDE (classic)

                Start the IDE and click on Help | About Freescale CodeWarrior.

                Click on Installed Products 

                Provide us all info displayed.

                Or you can save them in a txt file.

If the Installed Products is not available for older version you should find information in the welcome.txt

under the installation folder.

What is the Windows OS Used ?


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,348 次查看
kyleden
Contributor I

CodeWarrior for 68K Embedded Systems v3.2,

my OS is 64bit-win7。

in the “Obtaining Licenses ReadMe.txt” , there is the register E-mail "[email protected]",but it do not work.

:smileyconfused:first time to use the old version,thanks for help

0 项奖励
回复
2,349 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

I've installed CW for M68K v3.2 on  Win 7 64 bit OS and with the professional suite license, I can use the tool without problem.

What is the license file used ?

For this tool version, only the Professional Suite is available.

Attached you will find a temp license file.

This license file will expire the 15-nov-2015.

Rename the attached file to license.dat.

Have a great day,

Pascal

Freescale Technical Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,348 次查看
kyleden
Contributor I

Done! thank you !

0 项奖励
回复