License checkout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License checkout

1,453件の閲覧回数
wavesoftware
Contributor I

I have two floating licenses.  The last time I renewed them, I found that if I connected to the network and started Codewarrior, I could disconnect and compile and test without needing a network connection until the program crashed or I exited it.  However, at my most recent renewal, I now need to have network access to the license server to link my object at the end of compilation, every time.  My code size has increased, but it was too big previously to link without a license anyway, so I am unsure what has happened.

 

This restriction is really impacting my ability to do work in the field with quick turn arounds, as now I need to tether to a phone, VPN into the network, and hope that everything stays up as the code compiles, links and phones home.

 

Is there an option for converting one of my licenses to a dongle license, or is there a method I can check a license out for a few days for field work now and again?

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,301件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

please refer this article to rehost the license

How to rehost CodeWarrior suite license

if it can't work, please submit your case into the new system, please follow below steps:

1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.

2) On the bottom of the page under Submit New Issues, click Hardware & Software.

3) Register with your business email to access NXP technical online support.

4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.

5) On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信