License check failed: License server system does not support this feature.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

License check failed: License server system does not support this feature.

跳至解决方案
11,110 次查看
hpyovo
Contributor I

I want to use command tool which in cw_mpc5xxx_2.10\PowerPC_EABI_Tools\Command_Line_Tools\,but i find the linker license is failed,more info is below:

 

D:\Freescale\cw_mpc5xxx_2.10\PowerPC_EABI_Tools\Command_Line_Tools>mwasmeppc -fu

llLicenseSearch

### mwasmeppc Usage Error:

#   Nothing to do:  no source or object files specified

 

Errors caused tool to abort.

 

D:\Freescale\cw_mpc5xxx_2.10\PowerPC_EABI_Tools\Command_Line_Tools>mwcceppc -ful

lLicenseSearch

### mwcceppc Usage Error:

#   Nothing to do:  no source or object files specified

 

Errors caused tool to abort.

 

D:\Freescale\cw_mpc5xxx_2.10\PowerPC_EABI_Tools\Command_Line_Tools>mwldeppc -ful

lLicenseSearch

### mwldeppc Driver Error:

#   License check failed: License server system does not support this feature.

#   Feature:       Win32_Plugins_Link_PPC

#   License path:  D:\Freescale\cw_mpc5xxx_2.10\Bin\..\license.dat;

#   FLEXnet Licensing error:-18,147

#   For further information, refer to the FLEXnet Licensing documentation,

#   available at "www.macrovision.com".

 

Errors caused tool to abort.

 

The mwasmeppc and mwcceppc license is ok,but mwldeppc license failed, why?

 

I use LMTools Utility  Diagnostic Feature Win32_Plugins_Link_PPC, I got messege below:

 

License file: D:\Freescale\cw_mpc5xxx_2.10\license.dat

-----------------------------------------------------

"Win32_Plugins_Link_PPC" v8, vendor: metrowks

  License server: hpyovo-PC

  floating license no expiration date

 

  TS_OK: Checkout permitted when client is using terminal client

  Requests from the same USER/HOST do not consume a new license

 

This license can be checked out

-----------------------------------------------------

-----------------------------------------------------

License file: D:\Freescale\cw_mpc5xxx_2.10\PowerPC_EABI_Tools\Command_Line_Tools\license.dat

-----------------------------------------------------

No licenses for Win32_Plugins_Link_PPC in this license file

 

Anyone can help me, how do i fix the problem?

标签 (1)
0 项奖励
回复
1 解答
9,582 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi liu zq,

Sounds like they did not get a linker license increment in their license.dat file.  Please add this increment to the license.dat file:

INCREMENT Win32_Plugins_Link_PPC metrowks 8.000 30-may-2020 uncounted \

F41E210428AF VENDOR_STRING="PPC linker" HOSTID=ANY \

ISSUER="Freescale Semiconductor" ISSUED=17-apr-2012 NOTICE=N/A \

SN=N/A START=2-jan-2012 TS_OK

Should that not solve the issue, please submit a support request to the license team.

Regards,

在原帖中查看解决方案

0 项奖励
回复
3 回复数
9,583 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi liu zq,

Sounds like they did not get a linker license increment in their license.dat file.  Please add this increment to the license.dat file:

INCREMENT Win32_Plugins_Link_PPC metrowks 8.000 30-may-2020 uncounted \

F41E210428AF VENDOR_STRING="PPC linker" HOSTID=ANY \

ISSUER="Freescale Semiconductor" ISSUED=17-apr-2012 NOTICE=N/A \

SN=N/A START=2-jan-2012 TS_OK

Should that not solve the issue, please submit a support request to the license team.

Regards,

0 项奖励
回复
9,463 次查看
Duewee
Contributor I

Dear Jorge,

In the past I've successfully used the extension to my license.dat file below. However, I've noticed that this patch is not working anymore. The key seems to be expired since May 2020.

Can you provide me with an updated extension to my license file?

Best regards

0 项奖励
回复
9,572 次查看
hpyovo
Contributor I

Hi  jorge_plascencia,

I get the same wrong with your increment . I diagnostics the Win32_Plugins_Link_PPC,and i get the result below. 

I use command line,  the license still check failed such as below:

D:\Freescale\cw_mpc5xxx_2.10\PowerPC_EABI_Tools\Command_Line_Tools>mwldeppc -ful

lLicenseSearch

      1. mwldeppc Driver Error:

  1. License check failed: License server system does not support this feature.

  1. Feature: Win32_Plugins_Link_PPC

  1. License path: D:\Freescale\cw_mpc5xxx_2.10\Bin\..\license.dat ;

  1. FLEXnet Licensing error:-18,147

  1. For further information, refer to the FLEXnet Licensing documentation,

  1. available at "www.macrovision.com".

Errors caused tool to abort.

liuzq@hzepower.com

 From: jorge_plascenciaDate: 2016-06-14 03:41To: liu zqSubject: Re: - License check failed: License server system does not support this feature.

NXP Community

License check failed: License server system does not support this feature.

reply from jorge_plascencia in CodeWarrior Licensing - View the full discussion

Hi liu zq, Sounds like they did not get a linker license increment in their license.dat file.  Please add this increment to the license.dat file:  INCREMENT Win32_Plugins_Link_PPC metrowks 8.000 30-may-2020 uncounted \ F41E210428AF VENDOR_STRING="PPC linker" HOSTID=ANY \ ISSUER="Freescale Semiconductor" ISSUED=17-apr-2012 NOTICE=N/A \ SN=N/A START=2-jan-2012 TS_OK Should that not solve the issue, please submit a support request to the license team. Regards,

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in CodeWarrior Licensing by email or at NXP Community

Following License check failed: License server system does not support this feature. in these streams:

Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 项奖励
回复