Hello,
I am wondering if the license of CW for MPC55xx and MPC56xx 2.10 is working properly on the following environment.
environment
OS: Windows 7 (x64)
License Type: USB dongle (Node locked)
CW version: CW for MPC55xx and MPC56xx 2.10
FLEXId_D: version 11.9.1.0
lmtools: lmtools_x64_64bit_Windows (version 11.9.1.0)
解決済! 解決策の投稿を見る。
The so called classic edition of CodeWarrior do not extend support for dongle drivers in 64 bit Os.
However dongle is not a must, licenses are not limited to work with a dongle device.
You can choose between the dongle , Disk Serial or Ethernet MAC to be used as License reference.
If you need to move to other PC , you can generate different license in the NXP SW Licensing & Support screen.
My suggestion is to install in win 7 64 bit using disk serial num
The so called classic edition of CodeWarrior do not extend support for dongle drivers in 64 bit Os.
However dongle is not a must, licenses are not limited to work with a dongle device.
You can choose between the dongle , Disk Serial or Ethernet MAC to be used as License reference.
If you need to move to other PC , you can generate different license in the NXP SW Licensing & Support screen.
My suggestion is to install in win 7 64 bit using disk serial num