Does license of CW for MPC55xx and MPC56xx 2.10 work on Windows 7(x64)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does license of CW for MPC55xx and MPC56xx 2.10 work on Windows 7(x64)?

Jump to solution
1,062 Views
chunghohwang
Contributor II

Hello,

I am wondering if the license of CW for MPC55xx and MPC56xx 2.10 is working properly on the following environment.

environment

OS: Windows 7 (x64)

License Type: USB dongle (Node locked)

CW version: CW for MPC55xx and MPC56xx 2.10 

FLEXId_D:  version 11.9.1.0

lmtools: lmtools_x64_64bit_Windows (version 11.9.1.0)

0 Kudos
Reply
1 Solution
798 Views
TomasPaez
NXP Employee
NXP Employee

The so called classic edition of CodeWarrior do not extend support for dongle drivers in 64 bit Os.

However dongle is not a must, licenses are not limited to work with a dongle device.

You can choose between the dongle , Disk Serial or Ethernet MAC to be used as License reference.

If you need to move to other PC , you can generate different license in the NXP SW Licensing & Support screen.

My suggestion is to install in win 7 64 bit using disk serial num

View solution in original post

1 Reply
799 Views
TomasPaez
NXP Employee
NXP Employee

The so called classic edition of CodeWarrior do not extend support for dongle drivers in 64 bit Os.

However dongle is not a must, licenses are not limited to work with a dongle device.

You can choose between the dongle , Disk Serial or Ethernet MAC to be used as License reference.

If you need to move to other PC , you can generate different license in the NXP SW Licensing & Support screen.

My suggestion is to install in win 7 64 bit using disk serial num