DLA-STANDARD-FL license

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DLA-STANDARD-FL license

3,165 次查看
homereaton
Contributor I

Would like to run CodeWarrior using one computer at home and another one at the office but not concurrently. Is that possible with my FL license?

Homer

[email protected]

 

0 项奖励
回复
2 回复数

3,161 次查看
lisettelozano
NXP Employee
NXP Employee

Hello, 

Yes, it can be possible as soon as the home computer is connected to the same network (same IP range) as the server. It can be through VPN but, if the connection is not good, it will fail. 

Best Regards, 

Paulina

0 项奖励
回复

3,153 次查看
homereaton
Contributor I

Thank you very much for responding, Paulina.

Always used NL license before, first time with an FL.  My license.dat file generated doesn’t work. Read a lot of help on this but never found the help in inputting the correct settings for "Server Name / IP Address" and "Port" Do I get these settings from IPCONFIG /ALL data? Would very much appreciate your help. Can send you the license.dat file if that helps.

Thanks,

Homer

0 项奖励
回复