Code Warrior 5.1 do't show CAN components in PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior 5.1 do't show CAN components in PE

1,184 Views
Anonymous
Deactivated User

Dear Sir,

 

I have project in MC9s12G48 which have CAN component but it does't open in my CW5.1

I unable to see CAN component in processor expert .

 

Please help me.

Thanks in advance

 

rishi

Labels (1)
0 Kudos
Reply
1 Reply

1,071 Views
trytohelp
NXP Employee
NXP Employee

Hi,

I think you don't have the right license file.

There are 2 beans supporting the CAN:

    Init_MSCAN  under Peripheral Initialization Components which is included in all suites.

    FreescaleCAN is an Advanced Components which is included in Professional suite only.

You can order the bean separately too.

    Embedded Components|Freescale

By default under Processor Expert you've a "licensed" tab.

Only the beans validated by the license file are listed.

If you click on this tab you will have access to all beans.

However if you add the FreescaleCAN bean without having the right license file, no code will be generated for this bean.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply