Activated license not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activated license not working

2,645件の閲覧回数
denisdantas
Contributor II

Hello,

I currently have a paid license of the S12lisa toolchain but when I try to build our software, I get the following error:

"ERROR L4025: This limited version allows only 65536 bytes of C code"

When I open CodeWarrior and go to the Product Licenses window I can see that the license is activated (picture 1)

pastedImage_2.png

I also know that my makefile is linking to the correct license's path (picture 2)

pastedImage_3.png

In fact, the same project which I'm trying to build is being built by a colleague who also has the same license. I've been trying a few things to solve this but none worked so far. Any help on this issue will be very appreciated!

Best Regards,

Denis   

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,368件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello  Denis, 

This is indeed weird issue.

Could you please click on "Details" button and post the content here?

Can you attach also screenshot of  ERROR L4025 you get.

Thanks!

Stan

0 件の賞賛
返信

2,367件の閲覧回数
denisdantas
Contributor II

Issue solved. There was one environment variable missing.

0 件の賞賛
返信

2,367件の閲覧回数
stanish
NXP Employee
NXP Employee

Denis, Thanks for sharing the solution.

S.

0 件の賞賛
返信