SE052F with Qualcomm SEE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE052F with Qualcomm SEE

1,196件の閲覧回数
KiteJLKo
Contributor II

We need to develop the development guide for QSEE TrustApp (CA/TA) to enable Qualcomm SA522M to communicate with NXP's security chip via I2C in QSEE.

Planned Architecture: App<-->CA lib<---> TA<--->I2C<--->SE element(NXP SE052F)

1. Are there any relevant CA/TA development documents? Since we have no prior experience in this area, how can we obtain it?

2. Does NXP provide QSEE support code for the external security chip described above?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,183件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @KiteJLKo ,

 

No, we don't have any CA/TA development documents , actually SE052F accepts APDU commands complying with T=1 over I2C spec, and we provide MW to build user application, so if you build TA based on MW , there should be no issue with the planned Architecture. 
 
 
Hope that helps,
 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信