JCOP input capacitance of

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JCOP input capacitance of

1,356 Views
Barton
Contributor II

Does JCOP J3R452 has input capacitance?what's the input capacitance of JCOP J3R452 

Labels (2)
0 Kudos
Reply
1 Reply

1,333 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @Barton ,

 

Should be for JCOP 4.5 the input capacitor by default 56 pF.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply