Integrating customers smartcard infrastructure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrating customers smartcard infrastructure

2,368 Views
bwofsi
Contributor I

Hello,

We'd like to integrate with some customers smartcard infrastructure.
We cannot control which cards and standards are used and therefore would need an MCU that can read all cards possibly in use.
Private keys will be provided by the customers.
If we'd need several MCUs, please tell us the complete list.

Best wishes,
Fabiano

Labels (1)
0 Kudos
Reply
3 Replies

2,311 Views
bwofsi
Contributor I

Sorry for being unprecise. I meant contactless interface/smartcards.

0 Kudos
Reply

2,296 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bwofsi ,

 

Thanks for the clarification! I would recommend PN7642 for such case, which supports both of contact & contactless interfaces , with a M33 core inside, should be able to handle card reading tasks. Please kindly refer to https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/single-chip-solution-with-high-performance-... for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,354 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bwofsi ,

 

What kind of interface between the smartcard and MCU? is it a contact interface or contactless interface?

Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply