mpr121 raspberry pi help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpr121 raspberry pi help

3,406件の閲覧回数
rhubarbdog76
Contributor I

hi, 

I've bought a 12 key keypad which has an mpr121 chip built in.

How do i read registers 0x00 and 0x01?

How do i signal that the rq line has been read and can reset to high/floating?

i've got this far with the dummy method `keypad.rq_high

this is my python

import RPi.GPIO as GPIO
import posix
from fcntl import ioctl
import time

IOCTL_I2C_SLAVE = 0x0703

class KEYPAD:

  def __init__(self, i2c, rq_pin, address = 0x5a):
    self._fd = posix.open('/dev/i2c-%d' % i2c, posix.O_RDWR)
    ioctl(self._fd, IOCTL_I2C_SLAVE, address)

    self._rq_pin=rq_pin
    GPIO.setup(self._rq_pin, GPIO.IN, GPIO.PUD_UP)

    self.switch_on()

  def _del_(self):
    posix.close(self._fd)

  def switch_on(self):
    posix.write(self._fd, b'\x5e\x01')

  def rq_high(self):
    return GPIO.input(self._rq_pin) == GPIO.HIGH


GPIO.setmode(GPIO.BCM)

keypad=KEYPAD(1, 23)

try:

  while True:
    if keypad.rq_high():
      print("high", end = '\r')
    else:
      print("low ", end = '\r')

    time.sleep(0.01)

except KeyboardInterrupt:
    pass

print("")
GPIO.cleanup()

I only have switched on a few keys but realise i need to write something different to register 0x5e (probably 0x3f)

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

3,214件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Phil,

As you can see in the PCN16772, the MPR121 is a discontinued product and NXP no longer supports it.

However, attached you can find design guidelines including the sample code which might be helpful for your evaluation.

Best regards,

Tomas