Using Arduino interface of MIMX RT1170 EVK for sensor connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Arduino interface of MIMX RT1170 EVK for sensor connection

586 Views
SK02
Contributor I

Hello.

I am interfacing ultrasonic sensor to MIMX RT1170 EVK board. For interfacing the sensor I need to use Arduino interface for GPIOs connection. I am not able to find the proper connections for ultrasonic sensor connection, because not getting power at the pins.

I gave supply to board using adapter (J43). 
I need reference for pins connection and are there any settings required for powering ON the arduino interface region?

Thank you. 

0 Kudos
Reply
1 Reply

534 Views
mayliu1
NXP Employee
NXP Employee

Hi @SK02 ,

Thank you so much for your interest in our products and for using our community.

regarding your issue, could you please verify the following power configuration?

1: The adapter is connected to J43

2:  The SW5 power switch is turned ON

3: J38 is set to pins 1–2 to select the external 5 V input

Once these settings are confirmed, the board power rails—including those supplying the Arduino interface—should be available.

Please try it.

Best Regards

May

0 Kudos
Reply