TEF82xx CSI2 long package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEF82xx CSI2 long package

1,915件の閲覧回数
shansshi
Contributor I

Hello:

        The long packet contains a Packet Header (PH), application-specific data payload of a
variable number of 8-bit data words and a Packet Footer (PF).

        And The long packet PH consists an 8-bit data identifier. 

The value of PH data ID :0x30 to 0x37,these are used as user defined.

I want to know:

1、the range of data ID value mean the short packet?

2、the range of data ID value mean the long packet?

3、Are there other value of data ID, which  mean other packet?

4、we distinguish the short packet and long packet through the data ID?

5、Is TEF82xx CSI2 protocol different with standard CSI2?  IF different,where?

     shansshi_0-1652855419333.png

 

Thank you

 

  

0 件の賞賛
返信
2 返答(返信)

1,753件の閲覧回数
Hamanth
NXP Employee
NXP Employee

1、the range of data ID value mean the short packet?

Hamanth_0-1654085536029.png

Hamanth_6-1654085998863.png

 

2、the range of data ID value mean the long packet?

Hamanth_1-1654085766683.pngHamanth_2-1654085819098.pngHamanth_3-1654085849398.pngHamanth_4-1654085874243.pngHamanth_5-1654085897088.png

3、Are there other value of data ID, which  mean other packet?

No

4、we distinguish the short packet and long packet through the data ID?

Yes, Since all the synchronization packets have their own Data ID, It is used to distinguish between different types of packets

5、Is TEF82xx CSI2 protocol different with standard CSI2?  IF different,where?

No Differences

1,868件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have contacted our radar team, once I have answer I will feedback you.

Best regards,

Peter