TEF82xx CSI2 frame

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEF82xx CSI2 frame

1,945件の閲覧回数
shansshi
Contributor I

TEF82xx CSI2.pngHello:

we use the TEF82xx,It is used as FMCW RADAR transceiver.
And  we want to take the raw data to the fpga by the csi2. So we want to know the bits of the SoT、FS、EoT、PH、PF、FE、and so on.

 

Thank you.

0 件の賞賛
返信
4 返答(返信)

1,866件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As the TEF82xx information are mostly confidential it is not the best place to communicate it via community. If you are asking for such information, it is better to submit ticket on NXP web.

Have a look at reference manual of TEF82xx

chapter 4.2.2.7 CSI2 payload packet format and chapter 4.2.1.3 LVDS data format

Best regards,

Peter

0 件の賞賛
返信

1,939件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you share more info on this. Which micro you are referring to? Are you using Radar SDK?

Best regards,

Peter

0 件の賞賛
返信

1,908件の閲覧回数
shansshi
Contributor I

Hello,

        Can you give some infomation about our plan?

 

Thank you.

        

0 件の賞賛
返信

1,931件の閲覧回数
shansshi
Contributor I

Hello:

RF:TEF82xx.

FPGA:Lattice MD6000 or Xilinx XAZU5EV-1SFVC784Q, It is Connected with RF through the CSI2.

And we do not use Radar SDK.

So we want to know the frame protocol of the CSI2, for example the bits of the SoT、FS、EoT、PH、PF、FE, and so on.

0 件の賞賛
返信