Source not found error while debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source not found error while debugging

2,872 Views
TKB
Contributor II

Hi

I am completely new to using NXP microcontrollers. I am currently working with the FXTH870911. In order to understand the IDE better, I imported the TPMS_WheelLoc example project from the NXP website, compiled it and trying to debug now. 

This is where I placed my break point:

break_point.png

The first warning I get is:

TKB_5-1616515944452.png

 

I am using the PE Micro Multilink universal and the Port C - BDM to connect to the device. I am able to enter debug mode and step through the initial code. However once I try to step beyond the line PWUDIV = TPMS_LFOCAL(); I get the source not found error. See the image below.

TKB_1-1616515648073.png

On pressing F8 (continue), the program gets stuck below:

TKB_2-1616515726302.png

Just to be doubly sure, I tried the other available debug configuration and the result is the same.

TKB_3-1616515825741.png

Also, whenever I end the debug session and try to restart, I get the following message:

TKB_4-1616515887176.png

 

Can someone help me to understand what is going on here?

Thanks,

Tushar

 

0 Kudos
3 Replies

2,828 Views
TKB
Contributor II

Hi Tomas

Any updates on this?

Thanks

Tushar

0 Kudos

2,853 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

All you are describing here and seeing is actually normal. 

1. Breakpoint warning

The MCU only supports one breakpoint at a time. When the debug session is entered, the debugger automatically tries to place a breakpoint at the beginning of the main. But if you place a breakpoint before starting the debug session, then the debugger is unable to place a second breakpoint at the beginning of the main, since only one breakpoint at a time is supported, and warns the user with the pop up window “CodeWarrior Alert – Unable to set all breakpoints”. The consequence is that the user breakpoint is kept and no breakpoint is placed at the beginning of the main.

2. No source available / source not found

The FXTH device has a 16kByte flash, with 8kBytes programmed by NXP at production with an embedded firmware and 8kBytes reserved to the user application. The embedded firmware contains interrupt vectors, firmware functions described in the Firmware User Guide, and a jump table allowing the program to jump into the embedded firmware when the user application calls one of the firmware functions.

The CodeWarrior project developed by the user is intended for the user application flash section only, and does not have visibility on the embedded firmware programmed by NXP. It is thus not possible for the debugger to show the content of the embedded firmware because it does not have access to it, so it does not have access to the source code. This is why the message “No source available” or “No source found” is displayed.

3. Power Cycle Dialog

This message is normal and just indicates that the debugger is not able to force the MCU into background debug mode, which is necessary for programming and debugging. In this case it is necessary to do a hardware reset to allow the programming tool to force the MCU into background debug mode.

For new users like you, to get familiar with the FXTH family I would recommend the “Starter Package for FXTH87/E and MKW01” which can be downloaded from this webpage under “Development Software”. The package contains starter projects and documentation giving an overview of the device. The FXTH Documentation webpage also contains useful documents like manuals, user guides and app notes.

Hope it helps!

Best regards,

Tomas

0 Kudos

2,845 Views
TKB
Contributor II

Hi Tomas

Appreciate your help. 

1. Breakpoint warning makes sense now.

2. Source not found - The program is stuck here and I am not able to exit out to the next line in main.c. 

3. Power cycle dialog - Any reason why the soft reset is not working?

Thanks

Tushar

0 Kudos