Dear team,
I would like to ask about ODR accuracy of MMA8451Q.
My customer has a doubt on the accuracy of ODR(+-2%) from their test.
The customer’s test is as below.
As a result, they saw the interruption period from MMA8451Q could exceed from +-2%.
Is their test procedure is correct for ODR accuracy measurement?
Could you show me how to measure the ODR accuracy?
Best Regards,
Miyamoto
Solved! Go to Solution.
Hello Miyamoto-san,
Here is what I received from the product group:
The min max 4 sigma value is expected to be +/- 10%.
The best way is to measure using a DRDY interrupt as you mentioned. Measure the timing between them.
You can also use one of our kits (Sensor board + MCU) and our tools log data with timestamp. That can be the quickest way to get timestamp too.
It should be much better than 2% assuming no major temperature extremity.
We don’t have any data on aging accuracy but I don’t see it deviating more than +/- 10%.
Best regards,
Tomas
Hello TomasVaverka
Thanks for your support!
Could you show me what sigma values that the +/-2% of the typical value is?
Regards,
Miyamoto
Hello TomasVaverka
> We don’t have any data on aging accuracy but I don’t see it deviating more than +/- 10%.
The customer thinks that semi-conductor will not degrade then it will not be deviating more than +/- 10%. Right?
If so, do you have any documentations which can back up that?
Regards,
Miyamoto
Hello Miyamoto-san,
As mentioned before there are no documents about aging accuracy available.
Best regards,
Tomas
Hello TomasVaverka
Thanks for your reply!
How about the sigma number of the +/-2% typical value?
Regards,
Miyamoto
Hello Miyamoto-san,
I do not quite understand this question. The percentage should simply be a % of the ODR chosen. 2% of ODR 100 Hz should mean an expected deviation 2 Hz.
If this does not answer your question, please let me know.
Best regards,
Tomas
Hello TomasVaverka
You informed me about the MAX value is related to 4 sigma.
So the customer asked me that what sigma value is related to your typical +/-2%.
In my understanding, the sigma value is deeply related to the deviation in the viewpoint of statistics.
Regards,
Miyamoto
Hello Miyamoto-san,
Please find below what I got from our product group:
The min max 4 sigma value is expected to be +/- 10%. So, 1 sigma is basically 2.5% of ODR. That is the typical deviation. So, ODR +/- 2.5% is the typical ODR deviation (1 sigma).
4 sigma (10%) is the max you could get based on the oscillator.
Best regards,
Tomas
Dear Miyamoto-san,
Please note that ±2% is a typical value at 25 °C.
Although customer’s method makes sense, I would recommend a simpler technique without using the FIFO. Just select the ODR, enable the data ready interrupt (INT_EN_DRDY = 1), route it either to INT2 or INT1 (INT_CFG_DRDY = 0 or 1) and then measure changes on the selected INTx pin. .
I hope it helps.
Best regards,
Tomas
Hello Miyamoto-san,
I do apologize for the delay, I am double checking it with the product group and should have an answer by the end of this week.
Best regards,
Tomas
Hello TomasVaverka
Thanks, I will wait.
Please show me the MAX, MIN and aging of ODR accuracy.
Regards,
Miyamoto
Hello Miyamoto-san,
Here is what I received from the product group:
The min max 4 sigma value is expected to be +/- 10%.
The best way is to measure using a DRDY interrupt as you mentioned. Measure the timing between them.
You can also use one of our kits (Sensor board + MCU) and our tools log data with timestamp. That can be the quickest way to get timestamp too.
It should be much better than 2% assuming no major temperature extremity.
We don’t have any data on aging accuracy but I don’t see it deviating more than +/- 10%.
Best regards,
Tomas
Hello TomasVaverka
Thanks.
> Please note that ±2% is a typical value at 25 °C.
From below community thread, I understand that +2% is the Max.
Not true?
https://community.nxp.com/thread/436100
Please let me know the maximum value.
Anyway I will inform the customer the method you gave to me.
Regards,
Miyamoto