Pressure sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pressure sensor

2,082 Views
prasadbangar
Contributor I

Hi sir,

I have purchased MPXH6300AC6T1 Pressure sensor.My application is for measuring tyre pressure and i want to insert the sensor inside tubeless tyre which will be connected to the rim, the data is wireless transmitted and received through RF module and further processed by micro-controller,is MPXH6300AC6T1  suitable for placing it inside the Tyre and giving the precise results, if not

please suggest me some other IC which can  suit my application more focusing on placing sensor inside the tyre.


Thank you.

0 Kudos
1 Reply

1,940 Views
Joshevelle
Senior Contributor I

Hello Prasad,

Yes, you could use the MPXH6300A, however we have a dedicated product for this specific application, the FXTH870911D which has a pressure sensor, an accelerometer, RF transceiver and an S08 MCU integrated in a single 7x7mm package.

I would recommend you to take a look at the following demonstration video:

http://www.freescale.com/webapp/video_vault/videoSummary.sp?code=TPMS-DISPLAY-DEMO

Hope it helps.

-Josh

0 Kudos