PCF 8883

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF 8883

2,145件の閲覧回数
jangerrits
Contributor I

Hi, I'm currently working on a project for Capacitive Touch-sensor behind a 0.3 mm Steel Cover.

I was wondering if anybody has experience with such a project.

Is the PCF 8883 suitable for doing the job ?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,700件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Jan,

It should work properly, just an additional recommendation would be to avoid air gaps between the sensing plate and the dielectric (steel cover), in fact, if the sensing plate and the steel cover are touching this will increase the sensing area which means that the sensitivity would increase.

Here are some application notes that could be useful for this application:

AN10832 “PCF8883 and PCA8886 - capacitive proximity switch with auto-calibration” http://cache.nxp.com/documents/application_note/AN10832.pdf

AN11155 “General design guidelines for the NXP capacitive sensors” http://cache.nxp.com/documents/application_note/AN11155.pdf


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,700件の閲覧回数
jangerrits
Contributor I

Hi Jose

Thanks for your valuable answers it will help us a lot during the project !

Best regards and Have a nice day

Jan

Sent from iPad

Op 19 jan. 2016 om 22:04 heeft reyes <[email protected]<mailto:[email protected]>> het volgende geschreven:

NXP Community <http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1ty/3bt7M5ChS56s4_IVFJG9WA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQJ6kyiZ2Cef2qt-2B2uYN1YnWHaJNGi7m0dsLcrT7D0aEsRC9ydi8bGmPSoTrNqropzOzEJWlRcWGPjR3DG2V-2Fd9JgazgrYhAttaPsLKIUR-2FzQ-3D-3D>

PCF 8883

reply from Jose Alberto Reyes Morales<http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1ty/3bt7M5ChS56s4_IVFJG9WA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQnFOK00o-2FMItFkXWMeyx-2Fr-2BzmUjde-2BZny2kuFHrzaLsWAu7RZsM-2Bxn7-2B2e2pMMK9A-3D> in Sensors - View the full discussion<http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1ty/3bt7M5ChS56s4_IVFJG9WA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRIkJ0-2FxdZsf4dmjoFWbLvd2wKVAHG46aNpi1j8D3-2BDXOYfaINSEdo-2BM4Kef-2FDFK2Q-3D>

0 件の賞賛
返信