PCF 8883

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCF 8883

2,121 次查看
jangerrits
Contributor I

Hi, I'm currently working on a project for Capacitive Touch-sensor behind a 0.3 mm Steel Cover.

I was wondering if anybody has experience with such a project.

Is the PCF 8883 suitable for doing the job ?

标签 (1)
0 项奖励
回复
2 回复数

1,676 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Jan,

It should work properly, just an additional recommendation would be to avoid air gaps between the sensing plate and the dielectric (steel cover), in fact, if the sensing plate and the steel cover are touching this will increase the sensing area which means that the sensitivity would increase.

Here are some application notes that could be useful for this application:

AN10832 “PCF8883 and PCA8886 - capacitive proximity switch with auto-calibration” http://cache.nxp.com/documents/application_note/AN10832.pdf

AN11155 “General design guidelines for the NXP capacitive sensors” http://cache.nxp.com/documents/application_note/AN11155.pdf


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,676 次查看
jangerrits
Contributor I

Hi Jose

Thanks for your valuable answers it will help us a lot during the project !

Best regards and Have a nice day

Jan

Sent from iPad

Op 19 jan. 2016 om 22:04 heeft reyes <[email protected]<mailto:[email protected]>> het volgende geschreven:

NXP Community <http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1ty/3bt7M5ChS56s4_IVFJG9WA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQJ6kyiZ2Cef2qt-2B2uYN1YnWHaJNGi7m0dsLcrT7D0aEsRC9ydi8bGmPSoTrNqropzOzEJWlRcWGPjR3DG2V-2Fd9JgazgrYhAttaPsLKIUR-2FzQ-3D-3D>

PCF 8883

reply from Jose Alberto Reyes Morales<http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1ty/3bt7M5ChS56s4_IVFJG9WA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQnFOK00o-2FMItFkXWMeyx-2Fr-2BzmUjde-2BZny2kuFHrzaLsWAu7RZsM-2Bxn7-2B2e2pMMK9A-3D> in Sensors - View the full discussion<http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1ty/3bt7M5ChS56s4_IVFJG9WA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRIkJ0-2FxdZsf4dmjoFWbLvd2wKVAHG46aNpi1j8D3-2BDXOYfaINSEdo-2BM4Kef-2FDFK2Q-3D>

0 项奖励
回复