P3T1755 SDA Drive Levels ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P3T1755 SDA Drive Levels ?

7,484 次查看
smiller2
Contributor IV

I attempting to read the temperature via I3C at 12.5MHZ  from an FPGA implementation of the I3C controller.   The first byte is partially correct, but the send byte always reads as 0xFF.   It seems that on the transition of the read SDA line from High to Low, it takes too long and the P3T1755 detects a bogus Restart and places SDA into HiZ.     If I reduce the SCL frequency to 10MHZ with a 60nS clock low time, then it works as expected. 

Looking at the scope traces, the SDA line drive during reads seems quite weak when compared to some other devices.    I will attempt to attach scope shots of the working and non-working cases.  

Is there a spec on this drive strength?    Is there a command to increase it? 

 

Thanks.

 

0 项奖励
回复
5 回复数

7,458 次查看
smiller2
Contributor IV

The schematic goes across several boards, so it is not easy to share.   The SDA and SCL lines are FPGA pins with 1K pullups at the FPGA.  The signals route through several boards and have additional 1K pullups close to the P3T1755 sensor.     I am doing a Private Read command to retrieve the temperature.    I will attach some logic analyzer screen shots.  In the fail case, the logic analyzer is detecting that the SDA line transitioned HIGH while the SCL was already HIGH and is decoding as a STOP condition.    The P3T1755 has control of the SDA line at this time, so the issues are the prop delay in the SDA level change and the drive strength of the SDA line.    The datasheet does not seem to address the drive strength.  

0 项奖励
回复

7,432 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI Smiller

What's the communicate distance between sensor and controller?

If the long distance also can't support the maximum speed.

 

 

 

 

0 项奖励
回复

7,417 次查看
smiller2
Contributor IV

The FPGA is on a separate board.   There is probably 24 inches of PCB trace and two connector sets between the FPGA and the sensor.

0 项奖励
回复

7,404 次查看
guoweisun
NXP TechSupport
NXP TechSupport
0 项奖励
回复

7,470 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI Stephen 

Could you please share with the test waveforms and your schematic here?

 

Thanks!

0 项奖励
回复