No module named cli.cli - ssscli SE05X MW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No module named cli.cli - ssscli SE05X MW

1,666 Views
WorkerEmbedded
Contributor II

I'm trying to run ssscli from Plug and Trust MW, i've followed the documentation for install che cli and i'm stuck into this error. I've installed PyCli  an the error from "No module named 'cli'" become this:

File "<frozen runpy>", line 198, in _run_module_as_main
File "<frozen runpy>", line 88, in _run_code

File "C:\Users\%USER%\AppData\Roaming\Python\Python311-32\Scripts\ssscli.exe\__main__.py", line 4, in <module>
ModuleNotFoundError: No module named 'cli.cli'

Somebody have any solution?

Tags (3)
0 Kudos
Reply
1 Reply

1,621 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @WorkerEmbedded ,

 

Did you have the issue following the steps listed in simw-top/doc/pycli/doc/pre-steps.html#windows ? If yes, can you tell me in which step the issue happened? Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply