NXP20P0477 || Moisture Sensor || Abnormal Behavior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP20P0477 || Moisture Sensor || Abnormal Behavior

5,547 次查看
JyotiVaishnav
Contributor II

Hi NXP Team, 


We're using the NXP20P0477 IC on our board, and we're encountering an issue with its abnormal behavior. Even when no fault is present, it sometimes incorrectly shows a fault, and the FLAG signal goes low. At Controller end we are not using CC2 IC it is NM 

JyotiVaishnav_1-1745998144539.png

Please check the below Moisture IC schematic FYR

JyotiVaishnav_0-1745998080739.png

 

 

 

0 项奖励
回复
12 回复数

5,496 次查看
JyotiVaishnav
Contributor II

Hell Tomas,

One more query i need to address here , the marking on the IC which we are using in our current project is N7710022934 ,and the marking on the ic which we used in our previous project (were Ic is working properly , no false moisture detection)is N775911z234.
Why there is different marking in the IC ?, we have used same part no .

Please help us to answer this query , i just want to cross check whether there is no issue in the IC itself .


0 项奖励
回复

5,367 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jyoti,

I am still waiting for feedback from our product/test group, in the meantime could you please place the known-good (N775911z234) IC onto a board where the current lot shows false detection? If it works fine, the issue is definitely IC batch-related.

Also, could you please try to tie CC2 to GND through a pull-down resistor? 

BRs, Tomas

0 项奖励
回复

5,357 次查看
JyotiVaishnav
Contributor II

Hi Tomas, 

The 1kΩ pull-down resistor is specified on the CC2 line. Do you have any recommendations for the pull-down resistor value? Please share your input if there are any suggested values. Also, please see the image below. Meanwhile will check after changing the IC 

JyotiVaishnav_0-1746532957474.png

 

 

0 项奖励
回复

5,339 次查看
JyotiVaishnav
Contributor II

Hi,

Is there any difference in any of the LOT/BATCH CODE, please find the details below for both the LOT code mentioned below 

We are currently using this one and it is not working 

JyotiVaishnav_1-1746546630320.jpeg

And in our previous project we have used below part - and it is working fine 

JyotiVaishnav_2-1746546676177.jpeg

Please check and provide us the details for the LOT/BATCH code difference. 

 

 

0 项奖励
回复

5,310 次查看
JyotiVaishnav
Contributor II

Hi Tomas, 

Awaiting your response, our activities are blocked because of this.

Please check and provide the feedback. 

0 项奖励
回复

5,268 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Joyti,

The only feedback I have received so far from our product/test group is that "N775911z234" corresponds to WW34 of 2019 and "N7710022934" to WW34 of 2022. I am still waiting to hear if there are any functional differences between them or if there is any known issue with this newer batch (N7710022934).

BRs, Tomas

0 项奖励
回复

5,419 次查看
JyotiVaishnav
Contributor II

Hi Tomas, 

We are waiting your response here, please check and help us to debug the issue on an urgent a basis.

 

 

0 项奖励
回复

5,416 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jyoti,

Sorry for the delay in getting back to you, I have been out of the office the last few days. I will look into this with our product engineer later today and get back to you ASAP.

BRs, Tomas

 

0 项奖励
回复

5,387 次查看
JyotiVaishnav
Contributor II

Hi Tomas, 

We are waiting for your reply. 

We have measured the waveforms on the some of the test points, the detailed description is provided in the below attached document. Please refer the link to open the document. 

Password : e3PaWy78Ao
0 项奖励
回复

5,383 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jyoti,

Thank you for sharing additional details. I was able to download your presentation and will look into it with the product engineer soon.

BRs, Tomas

0 项奖励
回复

5,534 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jyoti,

FLAGB is an open-drain output and your schematic correctly uses a 100kOhm pull-up to 3.3V. It goes low when the device enters Moisture.DET state (COMP2 = high and COMP3 = low).

CP_EN is pulled-up to 3.3V via a 4.7kOhm resistor which enables the moisture detection logic.

Any noise or improper line status on CON_CCx can cause transitions into Moisture.DET state, especially during attach/detach events. So check for connector or routing noise that might mimic moisture. Also consider logging or probing CON_CC1/CC2 and CC1/CC2 voltages during failure.

BRs, Tomas

0 项奖励
回复

5,511 次查看
JyotiVaishnav
Contributor II

Hi Tomas, 

Please find the below waveform - measured on CC1 (IC input TP148)and FLAG (TP154 flag pin) in charging condition

JyotiVaishnav_1-1746082165164.png

below waveform - measured on CC1 (IC input TP148)and FLAG (TP154 flag pin) in moisture fault condition

JyotiVaishnav_3-1746082239265.png

Observation: As seen in the image above, a 350mV drift was observed on the CC line under fault conditions, and a moisture fault occurred after 4.3ms.

Please provide your suggestion to debug the issue 

0 项奖励
回复