MPR121 Touch detection start-up time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPR121 Touch detection start-up time

ソリューションへジャンプ
2,251件の閲覧回数
chaitanyamuppal
Contributor I

HI,

I am using MPR121 touch controller. It is taking  10 seconds time to detect touch, while GPIO control is happening immediate after power on.  I din't see anywhere in datasheet about start up time for MPR121 to detect touch.

Is there possibility to reduce this 10 seconds time by changing some config ??

ラベル(1)
1 解決策
1,716件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chaitanya,

This initial delay is caused by a large time constant of the baseline tracking filtering system. To reduce it, set both the CL (0x5E register) and BVA (0x7B register) bits to 0b10 or 0b11.

I hope it helps.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

元の投稿で解決策を見る

2 返答(返信)
1,717件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chaitanya,

This initial delay is caused by a large time constant of the baseline tracking filtering system. To reduce it, set both the CL (0x5E register) and BVA (0x7B register) bits to 0b10 or 0b11.

I hope it helps.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

1,716件の閲覧回数
chaitanyamuppal
Contributor I

Hi Tomas,

Now start-up time reduced to 4 sec by using above config. Thanks for your reply.

thanks,

chaitanya.

0 件の賞賛
返信