MPR031 HELP!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPR031 HELP!!!

3,016件の閲覧回数
rfslf
Contributor I

Please help me!
I use MPR031, and I can not start-up.

When I send 0x4A address, line is tied to ground and I cannot send command address.
When I send address from all range of possible, MPR031 does not respond.
MPR031 soldered well, contact is good. There is no answer from MPR031.

Please help me examples of an initial configuration of registers for MPR031.

 


Best regards,
Alex

0 件の賞賛
返信
2 返答(返信)

2,514件の閲覧回数
leo_oto
Contributor I

Did it work? I have the same problem. But it responds the adress but gets all zeros from EVERY register. Even if i write before i read. 

0 件の賞賛
返信

2,514件の閲覧回数
TomE
Specialist II

> I have the same problem. But it responds the adress..

 

Which is not the same problem. The original poster couldn't get a response at all.

 

Have you read the other posts in this forum on the MPR031 (and MPR121)?

 

Type "MPR031" into the Search Box and read the previous articles.

 

Tom

 

0 件の賞賛
返信