MMA8451 Fluctuation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8451 Fluctuation

8,011 Views
deepanrajanbara
Contributor IV

Hi ,

We are using mma8451 in our imx6 custom board.We tried following the instruction given in the below link for the register settings

How to use 2G, 4G, 8G modes in MMA8451Q Accelerometer? 

But doing the register setting there is fluctuation in the data obtained and we are not able come to one conclusion.

We have done all the setting as mentioned in https://community.nxp.com/docs/DOC-98836 

Is there anything we are missing so that the fluctuation in x,y,z data corrected.

Thank you,

Deepanraj.A

Labels (1)
0 Kudos
10 Replies

7,519 Views
deepanrajanbara
Contributor IV

The Driver which we are using is in the following path drivers/hwmon/mxc_mma8451.c

Is this driver correct ?

Thank you,

Deepanraj.A

0 Kudos

7,519 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Deepanraj,

Unfortunately I am not familiar with this driver, but I will try to find and look into it. Meanwhile, you may also try to use the i.MX community and ask others.

Best regards,

Tomas

0 Kudos

7,519 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Deepanraj,

It is hard to say where the problem might be. How much do your data fluctuate? Do you have a graph or a table illustrating it? Can you please also share your initialization and conversion routines?

Best regards,

Tomas

0 Kudos

7,519 Views
deepanrajanbara
Contributor IV

The register setting which we have followed are

XYZ_DATA_CFG set as 0x00

CTRL_REG2 set as 0x02

CTRL_REG1 set as 0x3D

The raw x , y and z data which is obtained we convert it to 14-bit data and divide by the sensitivity(4096) since the full scale is 2g as below

x = ((float)(ev[0].value>>2) / 4096)
y = ((float)(ev[1].value>>2) / 4096)
z = ((float)(ev[2].value>>2) / 4096)

The settings and raw data conversion is it proper ?

0 Kudos

7,519 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Deepanraj,

Yes, it appears to be correct. Just confirm that:

ev[0].value = OUT_X_MSB<<8 | OUT_X_LSB

ev[1].value = OUT_Y_MSB<<8 | OUT_Y_LSB

ev[2].value = OUT_Z_MSB<<8 | OUT_Z_LSB

As I asked before, can you please share the dataset showing the fluctuation?

Best regards,

Tomas

0 Kudos

7,517 Views
deepanrajanbara
Contributor IV

Hi Tomas,

As mentioned by you

ev[0].value = OUT_X_MSB<<8 | OUT_X_LSB

ev[1].value = OUT_Y_MSB<<8 | OUT_Y_LSB

ev[2].value = OUT_Z_MSB<<8 | OUT_Z_LSB

This operation is done.

Below is the attached raw data  of x,y and z which is got from accelerometer.

Thank you,

Deepanraj.A

0 Kudos

7,517 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Deepanraj,

The dataset you provided is really strange. You may have a defective part. Have you tested several MMA8451Q accelerometers or only one? How do you read the accel data (polling/interrupt)?

Best regards,

Tomas

0 Kudos

7,517 Views
deepanrajanbara
Contributor IV

Hi Tomas,

Is there a way to reduce this fluctuation by setting any of the registers ?

Thank you,

Deepanraj.A

0 Kudos

7,517 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Deepanraj,

Your register settings is correct (LNOISE = 1, MODS[1:0] = 0b11 = High resolution mode, ODR = 1.56Hz). Such a fluctuation, especially on the X and Y-axis, is not a noise. There must be another reason of such a variance, but I am currently not really sure what it might be.

Best regards,

Tomas

0 Kudos

7,517 Views
deepanrajanbara
Contributor IV

Hi Tomas,

We are following polling method and this is the data obtained from evtest application.

We also tested in another board with mma8451 sensor and found the same behavior.

The x and z axis seemed to be somewhat proper after the conversion But Y-Axis value is not proper

Thank you,

Deepanraj.A

0 Kudos