KMZ60 about start-up angle error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KMZ60 about start-up angle error

1,855件の閲覧回数
abcdchan15
Contributor I

I have question about KMZ60 application. I want to use it  to detect the position in Electronic throttle body. The datasheet mention about  " start-up angle error", the error is bigger with TC link to VCC.  Did i need to set the throttle to zero point to learn the zero point angle value for adjusting the error with every start-up, or just need once before  leaving the factory.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,570件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jianwei,

The KMZ60 does not have an automatic offset compensation integrated. That means, when you start the device, the output offset needs to be calibrated by your acquisition system.

Under standard conditions, it is sufficient to determine one time the Offset and TC-offset in fab and correct the KMZ60 signals with this offset vs. temperature characteristics.

Best regards,

Tomas

0 件の賞賛
返信