Is there any more information (Example code or application manual) about FXLS90322.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any more information (Example code or application manual) about FXLS90322.

2,041件の閲覧回数
lishihe142
Contributor I

@tomas Vaverka

ラベル(1)
0 件の賞賛
1 返信

1,983件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

Tomas is currently out of the office, but I can help.

 

FXLS90322 is a two channel DSI3, SPI and I2C compatible, lateral (X-Axis or Y-Axis) inertial, medium g ranges from ± 15.5 g to ± 150 g Nominal Full-Scale Range sensor.

 

This device is under pre-production status and we cannot share more detailed information about this product yet, I recommend you to contact your NXP Authorized distributor in case you need information about future availability of the product.

Regards,

Jose

NXP Semiconductors

0 件の賞賛