Is it possible to use PCF8883 for water level detection??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use PCF8883 for water level detection??

1,146件の閲覧回数
vijayendrakumar
Contributor I

Hi ,

Is it possible to use PCF8883 for water level detection?? Water column is building slowly in the container.

Regards,, 

ラベル(1)
0 件の賞賛
返信
1 返信

882件の閲覧回数
darioarias
NXP Employee
NXP Employee

Hello Vijayendra,

Could you give more details on how you are planning to measure the water level?

If your intention is to detect when water reaches certain point, I think that is possible, by placing an electrode on the fixed point and adjust the sensitivity of the PCF8883 to detect the change in capacitance that the water produce. If you want to put the electrode in the bottom and expect a change in capacitance as water rises, that's where I find it difficult because capacitance will remain the same.

Regards,

Darío

0 件の賞賛
返信