Information for part : MPXH6115A6T1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Information for part : MPXH6115A6T1

864 次查看
anilpatro
Contributor I

Please provide the recommended reflow profile temperature for sensor MPXH6115A6T1 - NXP (ex. Freescale). On the website it's only the peak temperature 250°C, but we need also the following details which could be found in reflow profile temperature graphic.

- Preheat temperatures.
- Preheat time
- Peak temperatures.
- Peak time.
- Ramp up/down
- Time above 200C

0 项奖励
回复
1 回复

801 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Anil,

Regarding soldering recommendations please refer to our AN3150 - Soldering Recommendations for Pressure Sensor Devices.

 

The reflow temperature profile for this device must be in accordance with J-STD-020C standart.

Best regards,

Tomas

0 项奖励
回复