Human Touch Detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Human Touch Detection

2,723件の閲覧回数
emekcanaras
Contributor I

Hi everyone,

I want to only detect human touch with my mpr121 sensor.For example when I make touch with a metal object , mpr121 detects.I need to ignore these kind of touches.Is there anything to do with mpr121 registers?Do I have to change electrode design?Any ideas?

ラベル(1)
0 件の賞賛
返信
1 返信

1,868件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

In most touch sensing applications the human finger is considered as one of the capacitor plates, while the conductive electrode is the complementary plate. This assumption is valid only if the human and the touch sensing device use the same potential reference, that is, only when the touch sensing device is physically grounded. An example of this user scenario is when a human is standing on the floor of their house touching the panel of an appliance that is physically grounded.

Make sure that the metalized piece that will be doing the touch is grounded, otherwise, you will need to perform your own tests, since we cannot warranty the correct behavior of the touch measurement, it’s true that it will alter the capacitance, but also there could be other factors (like environment) that could affect the performance of the sensor if the metal piece is not grounded.

However, also take in mind that our baseline algorithms will adjust over capacitive variations, include temperature, voltage, humidity (as long as it’s only humidity and not water droplets, which are a whole other thing), etc.

So, it would be very difficult for the MPR121 to distinguish between a human touch and a metal touch detections, but you can probably test with different metal sizes and a human finger touch, the best approach is to use grounded metal pins with a flat surface with different areas (for example, different sizes of screw heads) to try to identify the small difference between different metal touch and human finger touch and set the thresholds according to these differences. I cannot warranty that it can work since we have never tested before.

You can probably find further information in the following application note AN3863: http://cache.freescale.com/files/sensors/doc/app_note/AN3863.pdf

Regards,

Jose

0 件の賞賛
返信