Freedom Sensortoolbox Rev. 2.3 not working?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freedom Sensortoolbox Rev. 2.3 not working?

2,260件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi,

has anyone successfully installed and run the new release (Rev. 2.3) of the Freedom Sensor Toolbox?

I worked with an older version (Rev 2.1) before without any issues. Now with the updated release I can not run the "Kinetis Interface Tool" anymore.

I have Win7, 64-bit.

 

Any idea what's going wrong?

 

br

Guenter

42431_42431.PNGCapture.PNG

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-STBC-AGM01&fpsp=1&tab=Design_Too...#

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,593件の閲覧回数
aswins
NXP Employee
NXP Employee

Hi Guenter,

                 Can you elaborate your problem a little more please?. Is it like you are able to install REV 2.3 but you are getting error when you try to open Kinetis Interface Toolkit? Where in the installation process are you getting the error?

Thanks

Aswin

0 件の賞賛
返信

1,593件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi Aswin,

there was no error during the install process. The error appeard when opening the Kinetis Interface Toolkit after installation. But I think the error is gone.

I've updated the software to Rev. 2.3.2 today and it looks like it is working ok now.

I saw in the release notes that the error which I was confronted with has been fixed.

Thanks

Guenter

0 件の賞賛
返信

1,593件の閲覧回数
aswins
NXP Employee
NXP Employee

Hi Guenter,

              Glad that your problem is resolved .

Regards

Aswin

0 件の賞賛
返信