Current measure is noisy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Current measure is noisy

1,753 次查看
ext_jvi
Contributor I

Dear support / community,

I have tested the MM9Z_638 over a wide range of current, and after quite some debugging, it turned out that some noise on ISENSE is created by switching back and forth the TSENSE from internal temp to external temp (PTB3).

Curiously, I see a pick of error at a given current, depending on the PGA threshold configured for the current. With a certain configuration (3/16 and 13/16) we had a strong pick of error (>10A)  at 158A, which also increases with the temperature. 5A above or below, the error tends to disappear. Now with a different window of (14/16 and 2/16), the error is way smaller, but still noticeable, and now at about 440 A.

Is there a way to switch back and forth between internal temperature and external temperature (or voltage) without causing noise on the current measure ?

Kind regards,

Jean

标签 (1)
0 项奖励
回复
1 回复

1,592 次查看
Q_man
NXP Employee
NXP Employee

Hi Jean,

can you provide more details on external circuitry.

Thx

Wolfgang

0 项奖励
回复