Sensors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensors Knowledge Base

Discussions

Sort by:
This is a pre-release .msi installer for the Freescale Sensor Fusion Toolbox for Windows NEXT RELEASE.  This (or a later copy) will eventually replace the release copy at http://www.freescale.com/sensorfusion.  Altough this is a preview copy, it is believed stable.  Please let us know of any issues seen.  This version has a nice feature in that it can re-flash your Freedom board (KL25Z, KL26Z, KL46Z, K20D50M and K64F) with the matching firmware.  The new feature is under the File->Flash menu item.  There have also been some nice changes made to the "Magnetics" view.
View full article
The following video shows how to run the FRDM 6DOF Bare Board eCompass using the FRDM-K22. This algorithm uses the FXOS8700 contained on the Freedom Board. In order to get more information about the Sensor Fusion Library for Kinetis MCU's 5.0, please refer to the following link: Sensor Fusion|Freescale I hope this material will be useful for you. David
View full article
You will have to add a .exe extension to the unzipped file.
View full article
Issue Using the STB GUI for eCompass kits RD4247MAG3110 and RD4247FXOS8700 only -- v6.1.0.1 on a machine that does not have the Adobe Flash Player ActiveX program installed may run into the following error after pressing the eCompass button: Solution Install the Adobe Flash Player + ActiveX from Adobe. Let us know if you are facing any other issues with the STB GUI v6.1.0.1. Regards, Tomas
View full article
Attached is an LPCExpresso project for LPC1549.  It is compatible with the latest version of the Sensor Fusion Toolbox for Windows (the version targeted at Version 6.00 and 7.00 sensor fusion).  This project is a variant on the Sensor Fusion Version 6.00 library.  Algorithmically this is virtually identical to Version 7.00.
View full article
This posting summarizes known issues, not already in the errata) for Sensor Fusion Build 420: FRDM-KL25Z, KL26Z, KL46Z, K20D50M and K64F boards shipped to date do not include pull-up resistors on the NMI pin.  This has reportedly caused applications to not start properly because of inadvertent non-maskable interrupts.   There are several possible ways to resolve this: Add the missing pull-up resistor Disable the NMI during the first call to the NMI interrupt handler.  You can do that by replacing the existing default handler with:          // called on NMI          void Cpu_OnNMIINT(void)          {            // Disable NMI pin (some boards do not have pullups)            SIM_SCGC5 |= (uint32_t)SIM_SCGC5_PORTA_MASK; /* NMI and PORTA clock gate enable */            PORTA_PCR4 &= PORT_PCR_MUX_MASK;            /* enable input with pull up enable not NMI */            PORTA_PCR4 |= PORT_PCR_MUX(01) | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;            // return with no action            return;          } Add two new PE components.  One of type BitIO_LDD and the other of type Init_GPIO.  Between them you can assign PTA4 as an input GPIO with pullup enabled.  This has the advantage of requiring no changes to the .c or .h files. KDS builds using optimization level O3 do not properly execute the command interpreter within Events.c function UART_OnBlockReceived().  Change the project settings optimization level to O1 and it should work fine. It is possible for the Sensor Fusion Toolbox (both Windows and Android versions) to "fall out of sync" with the development board firmware with regard to desired sensor fusion algorithm being executed.  Symptoms and root causes are reviewed in the PDF attached to this posting.
View full article
As we develop videos on Sensor subjects for posting to QUMU and YouTube, these guidelines are a quick reminder of some important production points to remember. These lessons are relevent for any video content we develop.
View full article
All, Twitter traffic revealed a need for PDF versions of the sensor fusion documentation.  Apologies for any inconvenience.  Our standard documents are in Word format (we make extensive use of the equation tools in Word), and we supply them in that same format to make it easy to reuse the material.  But for those who do not have Word, please see the attached PDF. Regards, Mike
View full article
All, Drop the attached into SDK_2.0_FRDM-KL25Z/boards/frdmkl25z_virtual_shield/issdk_examples/algorithms/sensorfusion/baremetal_sensor_fusion. Apologies for both the delay in posting and the fact that even though I thought I was linking to files elsewhere in the system, I ended up getting local copies built into this project.  Some of you may like that.  I don't particularly.  But as I've noted elsewhere, KDS and I have our differences... Regards, Mike
View full article
Here is the Installer file for the revision 4.2.0.8 of the Sensor Toolbox GUI
View full article
MEMS sensors are mechanical structure chips and easily damaged by shock or huge vibration. Sensor package trend is going to small size, and it is not easy to solder by hand on pcb to verify. In order to do sensor verification before FA process, it is necessary to use a tool to load the failed chips and use I2C/SPI to access sensor registers to check sensor function. This document introduces to use sensor fixture and toolbox for a simple sensor verify tool. It is easy to provide precise failed spec items by this tool and to speed-up FA process.
View full article
This document provides answers for some of the common questions received by the Technical Support team about some inquiries with the usage of the CRTOUCH GUI.
View full article
Here's a zip file which incorporates the patch I outlined in my previous posting.
View full article
Video clip associated with "Android as a Platform for Sensor Fusion Education and Evaluation" presented at 2013 Sensors Expo & Conference by Michael Stanley.
View full article
Unibody Package with Axial Single Port Case 867F-03
View full article
List of software examples published by NXP technical support: Sensors software examples published by NXP technical support * List of breakout boards designed by NXP technical support: Freescale Sensors Breakout Boards Designs – HOME * All of the source code placed in spaces above is for example use only. NXP does not accept liability for use of this code in the user’s application.
View full article
Android sensor fusion APK
View full article
clicktaleID