Sensors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensors Knowledge Base

Discussions

Sort by:
Hands-on Training using Sensors Development Ecosystem
View full article
Here is the Installer file for the revision 4.2.0.8 of the Sensor Toolbox GUI
View full article
The MMA8491Q is a low voltage, 3-axis low-g accelerometer housed in a 3 mm x 3 mm QFN package. The device can accommodate two accelerometer configurations, acting as either a 45° tilt sensor or a digital output accelerometer with I2C bus.      • As a 45° Tilt Sensor, the MMA8491Q device offers extreme ease of implementation by using a single line output per axis.      • As a digital output accelerometer, the 14-bit ±8g accelerometer data can be read from the device with a 1 mg/LSB sensitivity. The extreme low power capabilities of the MMA8491Q will reduce the low data rate current consumption to less than 400 nA per Hz. Here is a Render of the MMA8491 Breakout Board downloaded from OSH park: Layout Design for this board: If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME
View full article
Hi Everyone, In this document I would like to go through a simple example code I created for the FRDMKL25-A8471 kit using the KDS 3.0.2 and KSDK 2.0. I will not cover the Sensor Toolbox – CE and Intelligent Sensing Framework (ISF) which primarily support this kit. The FreeMASTER tool is used to visualize the acceleration data that are read from the FXLS8471Q using an interrupt technique through the SPI interface. This example illustrates: 1. Initialization of the MKL25Z128 MCU (mainly PORT and SPI modules). 2. SPI data write and read operations. 3. Initialization of the FXLS8471Q to achieve the highest resolution. 4. Output data reading using an interrupt technique. 5. Conversion of the output values from registers 0x01 – 0x06 to real acceleration values in g’s. 6. Visualization of the output values in the FreeMASTER tool. 1. As you can see in the FRDMSTBC-A8471/FRDM-KL25Z schematics and the image below, SPI signals are routed to the SPI0 module of the KL25Z MCU and the INT1 output is connected to the PTD4 pin. The PTD0 pin (Chip Select) is not controlled automatically by SPI0 module, hence it is configured as a general-purpose output. The INT1 output of the FXLS8471Q is configured as a push-pull active-low output, so the corresponding PTD4 pin configuration is GPIO with an interrupt on falling edge. The configuration is done in the BOARD_InitPins() function using the NXP Pins Tool for Kinetis MCUs. void BOARD_InitPins(void) {    CLOCK_EnableClock(kCLOCK_PortD);                                          /* Port D Clock Gate Control: Clock enabled */    CLOCK_EnableClock(kCLOCK_Spi0);                                           /* SPI0 Clock Gate Control: Clock enabled */    PORT_SetPinMux(PORTD, PIN1_IDX, kPORT_MuxAlt2);                           /* PORTD1 (pin 74) is configured as SPI0_SCK */    PORT_SetPinMux(PORTD, PIN2_IDX, kPORT_MuxAlt2);                           /* PORTD2 (pin 75) is configured as SPI0_MOSI */    PORT_SetPinMux(PORTD, PIN3_IDX, kPORT_MuxAlt2);                           /* PORTD3 (pin 76) is configured as SPI0_MISO */    PORT_SetPinMux(PORTD, PIN0_IDX, kPORT_MuxAsGpio);                         /* PORTD0 (pin 73) is configured as PTD0 */    GPIO_PinInit(GPIOD, PIN0_IDX, &CS_config);                                /* PTD0 = 1 (Chip Select inactive) */       PORT_SetPinMux(PORTD, PIN4_IDX , kPORT_MuxAsGpio);                        /* PORTD4 (pin 77) is configured as PTD4 */    PORT_SetPinInterruptConfig(PORTD, PIN4_IDX, kPORT_InterruptFallingEdge);  /* PTD4 is configured for falling edge interrupts */      NVIC_EnableIRQ(PORTD_IRQn);                                               /* Enable PORTD interrupt on NVIC */ } The SPI_INIT() function is used to enable and configure the SPI0 module. The FXLS8471Q uses the ‘Mode 0′ SPI protocol, which means that an inactive state of clock signal is low and data are captured on the leading edge of clock signal and changed on the falling edge. The SPI clock is 500 kHz. void SPI_Init(void) {    uint32_t sourceClock = 0U;    sourceClock = CLOCK_GetFreq(kCLOCK_BusClk);    spi_master_config_t masterConfig = {    .enableMaster = true,    .enableStopInWaitMode = false,    .polarity = kSPI_ClockPolarityActiveHigh,    .phase = kSPI_ClockPhaseFirstEdge,    .direction = kSPI_MsbFirst,    .outputMode = kSPI_SlaveSelectAsGpio,    .pinMode = kSPI_PinModeNormal,    .baudRate_Bps = 500000U     };    SPI_MasterInit(SPI0, &masterConfig, sourceClock); } 2. The falling edge on the CS pin starts the SPI communication. A write operation is initiated by transmitting a 1 for the R/W bit. Then the 8-bit register address, ADDR[7:0] is encoded in the first and second serialized bytes. Data to be written starts in the third serialized byte. The order of the bits is as follows: Byte 0: R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0] Byte 1: ADDR[7], X, X, X, X, X, X, X Byte 2: DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0] The rising edge on the CS pin stops the SPI communication. Below is the write operation which writes the value 0x3D to the CTRL_REG1 (0x3A). Similarly a read operation is initiated by transmitting a 0 for the R/W bit. Then the 8-bit register address, ADDR[7:0] is encoded in the first and second serialized bytes. The data is read from the MISO pin (MSB first). The screenshot below shows the read operation which reads the correct value 0x6A from the WHO_AM_I register (0x0D). Multiple read operations are performed similar to single read except bytes are read in multiples of eight SCLK cycles. The register address is auto incremented so that every eighth next clock edges will latch the MSB of the next register. A burst read of 6 bytes from registers 0x01 to 0x06 is shown below. It also shows how the INT1 pin is automatically cleared by reading the acceleration output data. 3. At the beginning of the initialization, all FXLS8471Q registers are reset to their default values by setting the RST bit of the CTRL_REG2 register. The dynamic range is set to ±2g and to achieve the highest resolution, the LNOISE bit is set and the lowest ODR (1.56Hz) and the High Resolution mode are selected (more details in AN4075). The DRDY interrupt is enabled and routed to the INT1 interrupt pin that is configured to be a push-pull, active-low output. void FXLS8471Q_Init (void) {    FXLS8471Q_WriteRegister(CTRL_REG2, 0x40);            /* Reset all registers to POR values */    Pause(0xC62);                                        /* ~1ms delay */    FXLS8471Q_WriteRegister(CTRL_REG2, 0x02);            /* High Resolution mode */    FXLS8471Q_WriteRegister(CTRL_REG3, 0x00);            /* Push-pull, active low interrupt */    FXLS8471Q_WriteRegister(CTRL_REG4, 0x01);            /* Enable DRDY interrupt */    FXLS8471Q_WriteRegister(CTRL_REG5, 0x01);            /* DRDY interrupt routed to INT1 - PTD4 */    FXLS8471Q_WriteRegister(CTRL_REG1, 0x3D);            /* ODR = 1.56Hz, Reduced noise, Active mode */ } 4. In the ISR, only the interrupt flag is cleared and the DataReady variable is set to indicate the arrival of new data. void PORTD_IRQHandler(void) {    PORT_ClearPinsInterruptFlags(PORTD, 1<<4);           /* Clear the interrupt flag */    DataReady = 1; } 5. In the main loop, the DataReady variable is periodically checked and if it is set, the accelerometer registers 0x01 – 0x06 are read and then converted to signed 14-bit values and real values in g’s. if (DataReady)                                                        /* Is a new set of data ready? */ {    DataReady = 0;    FXLS8471Q_ReadMultiRegisters(OUT_X_MSB_REG, 6, AccData);           /* Read data output registers 0x01-0x06 */    Xout_14_bit = ((int16_t) (AccData[0]<<8 | AccData[1])) >> 2;       /* Compute 14-bit X-axis output value */    Yout_14_bit = ((int16_t) (AccData[2]<<8 | AccData[3])) >> 2;       /* Compute 14-bit Y-axis output value */    Zout_14_bit = ((int16_t) (AccData[4]<<8 | AccData[5])) >> 2;       /* Compute 14-bit Z-axis output value */    Xout_g = ((float) Xout_14_bit) / SENSITIVITY_2G;                   /* Compute X-axis output value in g's */    Yout_g = ((float) Yout_14_bit) / SENSITIVITY_2G;                   /* Compute Y-axis output value in g's */    Zout_g = ((float) Zout_14_bit) / SENSITIVITY_2G;                   /* Compute Z-axis output value in g's */ } 6. The calculated values can be watched in the Debug perspective or in the FreeMASTER application. To open and run the FreeMASTER project, install the FreeMASTER 2.0 application and FreeMASTER Communication Driver. Attached you can find the complete source code written in the KDS 3.0.2 including the FreeMASTER project. If there are any questions regarding this simple application, do not hesitate to ask below. Your feedback or suggestions are also welcome. Best regards, Tomas
View full article
My friend Matt Muddiman of Freescale gave this presentation as part of the MEMS Education Series (hosted by Arizona Technology Council and MEMS Industry Group) in Scottsdale Arizona earlier this week.
View full article
Hi Everyone, This tutorial is a detailed guide on how to import an ISSDK based example project (e.g. mma845x_interrupt) into MCUXpresso IDE, build and run it on the Freedom board (e.g. FRDM-KL27Z). If you intend to use another ISSDK example project/board, you can always follow this guide. A complete list of MCU boards, sensor kits and sensors supported by ISSDK is available in the ISSDK Release notes. 1. Download the FRDM-KL27Z SDK Open a web browser, navigate to the MCUXpresso homepage and select “Login to view configurations” to start a new configuration. You will be redirected to login to nxp.com. Enter your account information or register for a new account. Back on the MCUXpresso homepage, select the drop-down box to create a New Configuration. Select the board (FRDM-KL27Z) from the list and provide a name for the configuration. Select “Specify Additional Configuration Settings” to choose the Host OS, Toolchain (MCUXpresso IDE) and Middleware (ISSDK). Select Configuration Settings: Host OS (example: Windows) Toolchain/IDE (MCUXpresso IDE) Middleware (ISSDK) Once the configurations are set, select “Go to SDK Builder”.   Select “Request Build” to download the SDK. Once the build request is completed, download the SDK. Agree to Software Terms and Conditions. Unzip SDK to a folder (e.g. SDK_2.2.1_FRDM-KL27Z). 2. Import the SDK_2.1.1_FRDM-KL27Z into MCUXpresso IDE Open MCUXpresso IDE. Set the workspace directory of your choice and click on OK. Switch to the Installed SDKs view within the MCUXpresso IDE window. Open Windows Explorer, and drag and drop the SDK_2.2.1_FRDM-KL27Z (unzipped) file into the installed SDKs view. You will get the following pop-up so click on OK to continue the import.   The installed SDK will appear in the Installed SDKs view. 3. Import and build the ISSDK based mma845x_interrupt example project Find the Quickstart Panel in the lower left hand corner and select Import SDK example(s) Click on the FRDM-KL27Z board and then click on Next. Use the arrow button to expand the issdk_examples category, and then click the checkbox next to mma845x_interrupt to select that project. Then, click on Next. On the next screen, click the checkbox to Redirect printf/scanf to UART so that the terminal output gets sent out the UART instead of using semi-hosting through the debugger. Then click on Finish. Now build the project by clicking on the project name in the Project Explorer view and then click on the Build icon in the Quickstart Panel. You can see the status of the build in the Console view. 4. Run the mma845x_interrupt example project   Now that the project has been compiled, we can flash it to the board and run it. Make sure the FRDM-KL27Z board is plugged in, and click on Debug ‘frdmkl27z_issdk_examples_sensors_mma8451q_mma845x_interrupt’ [Debug] MCUXpresso will probe for connected boards and should find the OpenSDA debug probe that is part of the integrated OpenSDA circuit on the FRDM-KL27Z board. Click on OK to continue. The firmware will be downloaded to the board and the debugger started. Open a Terminal program (e.g. Tera Term) and connect to the FRDM-KL27Z COM port that it enumerated as. Use 115200 baud, 8 data, 1 stop, no parity. Start the application in the MCUXpresso IDE by clicking the "Resume" button. The application is now running and signed 14-bit accelerometer output values are displayed on the terminal. To modify the initial register settings of the MMA8451 accelerometer, find the mma845x_Config_Isr[] structure and change it according to your needs. Well done if you managed to follow along and get it all working. If there are any questions, do not hesitate to ask below. Your feedback or suggestions are also welcome. Regards, Tomas
View full article
The attached is a copy of a presentation given 24 June 2014 at the Sensors Expo Conference in Rosemont IL.
View full article
"Android as a Platform for Sensor Fusion Education and Evaluation" presented at 2013 Sensors Expo & Conference by Michael Stanley.
View full article
Hi Everyone,   If you are interested in a simple bare metal example code illustrating the use of the FXLS8471Q orientation detection function, please find below one of my examples I created for the FXLS8471Q accelerometer while working with the NXP FRDM-KL25Z platform and FRDMSTBC-A8471 board.   This example code complements the code snippet from the  AN4068.   void FXLS8471Q_Init (void) { FXLS8471Q_WriteRegister(CTRL_REG1, 0x00); // Standby mode FXLS8471Q_WriteRegister(PL_CFG_REG, 0x40); // Enable orientation detection FXLS8471Q_WriteRegister(PL_BF_ZCOMP_REG, 0x43); // Back/Front trip point set to 75°, Z-lockout angle set to 25° FXLS8471Q_WriteRegister(P_L_THS_REG, 0x14); // Threshold angle = 45°, hysteresis = 14° FXLS8471Q_WriteRegister(PL_COUNT_REG, 0x05); // Debounce counter set to 100ms at 50Hz FXLS8471Q_WriteRegister(CTRL_REG3, 0x00); // Push-pull, active low interrupt FXLS8471Q_WriteRegister(CTRL_REG4, 0x10); // Orientation interrupt enabled FXLS8471Q_WriteRegister(CTRL_REG5, 0x10); // Route orientation interrupt to INT1 - PTD4 FXLS8471Q_WriteRegister(CTRL_REG1, 0x21); // ODR = 50Hz, Active mode }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍     In the ISR, only the interrupt flag is cleared and the PL_STATUS (0x10) register is read in order to:   - Clear the SRC_LNDPRT flag in the INT_SOURCE register and deassert the INT1 pin, as shown on the screenshot below. - Get orientation information. 0x82 in this example corresponds to "Portrait down" orientation.   void PORTD_IRQHandler() { PORTD_PCR4 |= PORT_PCR_ISF_MASK; // Clear the interrupt flag PL_Status = FXLS8471Q_ReadRegister(PL_STATUS_REG); // Read the PL_STATUS register to clear the SRC_LNDPRT flag in the INT_SOURCE register }‍‍‍‍‍‍‍‍‍‍       Attached you can find the complete source code. If there are any questions regarding this simple example code, please feel free to ask below.    Regards, Tomas
View full article
Hi Everyone, In my previous tutorial, I demonstrated how to import an ISSDK based example project into MCUXpresso IDE, build and run it on the Freedom board (FRDM-KL27Z). If you want to visualize/log sensor data, easily change sensor settings (ODR, Range, Power Mode) or directly read and write sensor registers, you can use the Freedom Sensor Toolbox-Community Edition (STB-CE) as described below or in the STBCEUG. 1. Connect the SDA port (J13) on the FRDM-KL27Z board to a USB port on your computer. 2. Open STB-CE GUI by double clicking the Freedom Sensor Toolbox (CE) shortcut located on your desktop. 3. Select "Out of Box Sensor Demonstration". 4. Select the Project to be launched and click on Continue. Base Board Name – FRDM-KL27Z Shield Board Name – OnBoard Project Name – MMA8451 Accelerometer Demo 5. The ISSDK-based MMA8451 Accelerometer Demo firmware is loaded to the KL27Z MCU and the MMA8451 Accelerometer Demo v1.0 GUI launched. 6. In the Main screen you can change basic MMA8451Q accelerometer settings (ODR, Range, Power Mode), enable embedded functions (Landsacpe/Portrait, Pulse/Tap, Freefall, Transient), start/stop accelerometer data streaming and/or logging.   7. The Register screen (MMA8451) provides low-level access (R/W) to the MMA8451Q registers along with a detailed description of the selected register. 8. To change the bit value, simply click on the corresponding cell (make sure you selected the Standby mode before writing a new value to the selected register). I hope you find this simple document useful. f there are any questions, please feel free to ask below.  Regards, Tomas
View full article
The MMA845xQ is a smart low-power, three-axis capacitive micromachined accelerometer up to 14 bits of resolution. This accelerometer is packed with embedded functions with flexible user-programmable options, configurable to two interrupt pins. Embedded interrupt functions allow for overall power savings relieving the host processor from continuously polling data. There is access to both low-pass filtered data as well as high-pass filtered data, which minimizes the data analysis required for jolt detection and faster transitions. The device can be configured to generate inertial wake-up interrupt signals from any combination of the configurable embedded functions allowing the MMA845xQ to monitor events and remain in a low-power mode during periods of inactivity. Here is a Render of the MMA845x Breakout- Board downloaded from OSH Park: And here is an image of the Layout Design for this board: In the Attachments section, you can find the Schematic Source File (.SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM for this Breakout-board. If you are interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME
View full article
The FXLN83XX is a 3-axis, low-power, low-g accelerometer along with a CMOS signal conditioning and control ASIC in a small 3 x 3 x 1 mm QFN package. The analog outputs for the X, Y, and Z axes are internally compensated for zero-g offset and sensitivity, and then buffered to the output pads. The outputs have a fixed 0 g offset of 0.75 V, irrespective of the VDD supply voltage. The bandwidth of the output signal for each axis may be independently set using external capacitors. The host can place the FXLN83XXQ into a low-current shutdown mode to conserve power. Here is a Render of the FXLN83XX Breakout Board downloaded from OSH park: Layout Design for this board: In the attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files.    If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOMEFreescale Sensors Breakout Boards Designs – HOME
View full article
Hi Everyone,   In this document I would like to go through a simple bare-metal example code I created for the recently released FRDMSTBC-A8471 development board with the NXP FXLS8471Q 3-axis linear accelerometer. This board is compatible with most NXP Freedom development boards and I decided to use one of the most popular - FRDM-KL25Z. The FreeMASTER tool is used to visualize the acceleration data that are read from the FXLS8471Q using an interrupt technique through the SPI interface. I will not cover the Sensor Toolbox software and Intelligent Sensing Framework (ISF) which also support this board.   This example illustrates:   1. Initialization of the MKL25Z128 MCU (mainly SPI and PORT modules). 2. SPI data write and read operations. 3. Initialization of the FXLS8471Q to achieve the highest resolution. 4. Simple offset calibration based on the AN4069. 5. Output data reading using an interrupt technique. 6. Conversion of the output values from registers 0x01 – 0x06 to real acceleration values in g’s. 7. Visualization of the output values in the FreeMASTER tool.     1. As you can see in the FRDMSTBC-A8471​/FRDM-KL25Z​ schematics and the image below, SPI signals are routed to the SPI0 module of the KL25Z MCU and the INT1 output is connected to the PTD4 pin. The PTD0 pin (Chip Select) is not controlled automatically by SPI0 module, hence it is configured as a general-purpose output. The INT1 output of the FXLS8471Q is configured as a push-pull active-low output, so the corresponding PTD4 pin configuration is GPIO with an interrupt on falling edge.The core/system clock frequency is 20.97 MHz and SPI clock is 524.25 kHz.     The MCU is, therefore, configured as follows.   /****************************************************************************** * MCU initialization function ******************************************************************************/   void MCU_Init(void) {   //SPI0 module initialization   SIM_SCGC4 |= SIM_SCGC4_SPI0_MASK; // Turn on clock to SPI0 module   SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK; // Turn on clock to Port D module   PORTD_PCR1 = PORT_PCR_MUX(0x02); // PTD1 pin is SPI0 CLK line   PORTD_PCR2 = PORT_PCR_MUX(0x02); // PTD2 pin is SPI0 MOSI line   PORTD_PCR3 = PORT_PCR_MUX(0x02); // PTD3 pin is SPI0 MISO line   PORTD_PCR0 = PORT_PCR_MUX(0x01); // PTD0 pin is configured as GPIO (CS line driven manually)   GPIOD_PSOR |= GPIO_PSOR_PTSO(0x01); // PTD0 = 1 (CS inactive)   GPIOD_PDDR |= GPIO_PDDR_PDD(0x01); // PTD0 pin is GPIO output     SPI0_C1 = SPI_C1_SPE_MASK | SPI_C1_MSTR_MASK; // Enable SPI0 module, master mode   SPI0_BR = SPI_BR_SPPR(0x04) | SPI_BR_SPR(0x02); // BaudRate = BusClock / ((SPPR+1) * 2^(SPR+1)) = 20970000 / ((4+1) * 2^(2+1)) = 524.25 kHz     //Configure the PTD4 pin (connected to the INT1 of the FXLS8471Q) for falling edge interrupts   PORTD_PCR4 |= (0|PORT_PCR_ISF_MASK| // Clear the interrupt flag                   PORT_PCR_MUX(0x1)| // PTD4 is configured as GPIO                   PORT_PCR_IRQC(0xA)); // PTD4 is configured for falling edge interrupts     //Enable PORTD interrupt on NVIC   NVIC_ICPR |= 1 << ((INT_PORTD - 16)%32);   NVIC_ISER |= 1 << ((INT_PORTD - 16)%32); }     2. The FXLS8471Q uses the ‘Mode 0′ SPI protocol, which means that an inactive state of clock signal is low and data are captured on the leading edge of clock signal and changed on the falling edge.   The falling edge on the CS pin starts the SPI communication. A write operation is initiated by transmitting a 1 for the R/W bit. Then the 8-bit register address, ADDR[7:0] is encoded in the first and second serialized bytes. Data to be written starts in the third serialized byte. The order of the bits is as follows:   Byte 0: R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0] Byte 1: ADDR[7], X, X, X, X, X, X, X Byte 2: DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0]   The rising edge on the CS pin stops the SPI communication.   Below is the write operation which writes the value 0x3D to the CTRL_REG1 (0x3A).   Similarly a read operation is initiated by transmitting a 0 for the R/W bit. Then the 8-bit register address, ADDR[7:0] is encoded in the first and second serialized bytes. The data is read from the MISO pin (MSB first).   The screenshot below shows the read operation which reads the correct value 0x6A from the WHO_AM_I register (0x0D).   Multiple read operations are performed similar to single read except bytes are read in multiples of eight SCLK cycles. The register address is auto incremented so that every eighth next clock edges will latch the MSB of the next register.   A burst read of 6 bytes from registers 0x01 to 0x06 is shown below. It also shows how the INT1 pin is automatically cleared by reading the acceleration output data.     3. The dynamic range is set to ±2g and to achieve the highest resolution, the LNOISE bit is set and the lowest ODR (1.56Hz) and the High Resolution mode are selected (more details in AN4075). The DRDY interrupt is enabled and routed to the INT1 interrupt pin that is configured to be a push-pull, active-low output.   /****************************************************************************** * FXLS8471Q initialization function ******************************************************************************/   void FXLS8471Q_Init (void) {   FXLS8471Q_WriteRegister(CTRL_REG2, 0x02); // High Resolution mode   FXLS8471Q_WriteRegister(CTRL_REG3, 0x00); // Push-pull, active low interrupt   FXLS8471Q_WriteRegister(CTRL_REG4, 0x01); // Enable DRDY interrupt   FXLS8471Q_WriteRegister(CTRL_REG5, 0x01); // DRDY interrupt routed to INT1-PTD4   FXLS8471Q_WriteRegister(CTRL_REG1, 0x3D); // ODR = 1.56Hz, Reduced noise, Active mode   }     4. A simple offset calibration method is implemented according to the AN4069​.   /****************************************************************************** * Simple accelerometer offset calibration ******************************************************************************/   void FXLS8471Q_Calibrate (void) {   unsigned char reg_val = 0;     while (!reg_val) // Wait for a first set of data    {     reg_val = FXLS8471Q_ReadRegister(STATUS_REG) & 0x08;   }      FXLS8471Q_ReadMultiRegisters(OUT_X_MSB_REG, 6, AccData); // Read data output registers 0x01-0x06       Xout_14_bit = ((short) (AccData[0]<<8 | AccData[1])) >> 2; // Compute 14-bit X-axis output value   Yout_14_bit = ((short) (AccData[2]<<8 | AccData[3])) >> 2; // Compute 14-bit Y-axis output value   Zout_14_bit = ((short) (AccData[4]<<8 | AccData[5])) >> 2; // Compute 14-bit Z-axis output value      Xoffset = Xout_14_bit / 8 * (-1); // Compute X-axis offset correction value   Yoffset = Yout_14_bit / 8 * (-1); // Compute Y-axis offset correction value   Zoffset = (Zout_14_bit - SENSITIVITY_2G) / 8 * (-1); // Compute Z-axis offset correction value      FXLS8471Q_WriteRegister(CTRL_REG1, 0x00); // Standby mode to allow writing to the offset registers   FXLS8471Q_WriteRegister(OFF_X_REG, Xoffset);   FXLS8471Q_WriteRegister(OFF_Y_REG, Yoffset);   FXLS8471Q_WriteRegister(OFF_Z_REG, Zoffset);      FXLS8471Q_WriteRegister(CTRL_REG1, 0x3D); // ODR = 1.56Hz, Reduced noise, Active mode }     5. In the ISR, only the interrupt flag is cleared and the DataReady variable is set to indicate the arrival of new data.   /****************************************************************************** * PORT D Interrupt handler ******************************************************************************/   void PORTD_IRQHandler() {   PORTD_PCR4 |= PORT_PCR_ISF_MASK; // Clear the interrupt flag   DataReady = 1; }     6. The output values from accelerometer registers 0x01 – 0x06 are first converted to signed 14-bit values and afterwards to real values in g’s.   if (DataReady)     // Is a new set of data ready? {   DataReady = 0;     FXLS8471Q_ReadMultiRegisters(OUT_X_MSB_REG, 6, AccData); // Read data output registers 0x01-0x06                                                    Xout_14_bit = ((short) (AccData[0]<<8 | AccData[1])) >> 2; // Compute 14-bit X-axis output value   Yout_14_bit = ((short) (AccData[2]<<8 | AccData[3])) >> 2; // Compute 14-bit Y-axis output value   Zout_14_bit = ((short) (AccData[4]<<8 | AccData[5])) >> 2; // Compute 14-bit Z-axis output value                                        Xout_g = ((float) Xout_14_bit) / SENSITIVITY_2G; // Compute X-axis output value in g's   Yout_g = ((float) Yout_14_bit) / SENSITIVITY_2G; // Compute Y-axis output value in g's   Zout_g = ((float) Zout_14_bit) / SENSITIVITY_2G; // Compute Z-axis output value in g's }     7. The calculated values can be watched in the "Variables" window on the top right of the Debug perspective or in the FreeMASTER application. To open and run the FreeMASTER project, install the FreeMASTER 2.0 application and FreeMASTER Communication Driver.         Attached you can find the complete source code written in the CW for MCU's v10.6​ including the FreeMASTER project.   If there are any questions regarding this simple application, please feel free to ask below. Your feedback or suggestions are also welcome.   Regards, Tomas
View full article
Hi, The MMA865x, 3-axis, 10-bit/12-bit accelerometer that has industry leading performance in a small 2 x 2 x 1 mm DFN package. This accelerometer is packed with embedded functions that include flexible user-programmable options and two configurable interrupt pins. Overall power savings is achieved through inertial wake-up interrupt signals that monitor events and remain in a low-power mode during periods of inactivity. Here is a Render of the MMA865x Breakout- Board downloaded from OSH park: Layout Design for this board: In the attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files. If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME
View full article
Video clip associated with "Android as a Platform for Sensor Fusion Education and Evaluation" presented at 2013 Sensors Expo & Conference by Michael Stanley.
View full article
The MMA690x, a SafeAssure solution, is a dual axis, Low g, XY, Sensorbased on Freescale’s HARMEMS technology, with an embedded DSP ASIC, allowing for additional processing of the digital signals. Here is a Render of the MMA690x Breakout Board downloaded from OSH park: Layout Design for this board: In the attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files.   If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOME
View full article
Hi Everyone,   I would like to present another example code/demo that reads acceleration data from the Xtrinsic MMA8491Q digital accelerometer and visualizes them using the FreeMASTER tool via USBDM interface. I have used recently released Xtrinsic MEMS sensors board that features three types of Xtrinsic sensors including the MMA8491Q and is fully compatible with the Freescale FRDM-KL25Z platform.   In comparison with other Xtrinsic accelerometers, the MMA8491Q is turned on at the rising edge on the EN pin and acquires only one sample for each of the three axes. It does not have any interrupt pins, instead there are three push-pull logic outputs which provide tilt detection at 45 degrees as the original target application was tamper detection. However, it is possible to read the 14-bit output values through the I2C port as demonstrated in my example below.   According to the User Manual, both SCL and SDA lines are connected through the 4.7K pull-up resistors to the I2C1 module (PTE1 and PTE0 pins) on the KL25Z128 MCU and the EN pin is connected to the PTA13 pin. The EN input needs to be kept high until a new data is ready (max. 900us) and read. In my code I use the PIT module to wait 1ms before reading the output values. This timer is also used to read the output data periodically at a fixed rate. The timeout period of the PIT is set to 500us. The MCU is, therefore, configured as follows:   void MCU_Init(void) {             //I2C1 module initialization             SIM_SCGC4 |= SIM_SCGC4_I2C1_MASK;        // Turn on clock to I2C1 module         SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK;       // Turn on clock to Port E module        PORTE_PCR1 = PORT_PCR_MUX(6);            // PTE1 pin is I2C1 SCL line        PORTE_PCR0 = PORT_PCR_MUX(6);            // PTE0 pin is I2C1 SDA line        I2C1_F  = 0x14;                          // SDA hold time = 2.125us, SCL start hold time = 4.25us, SCL stop hold time = 5.125us         I2C1_C1 = I2C_C1_IICEN_MASK;             // Enable I2C1 module                //Configure the PTA13 pin as an output to drive the EN input of the MMA8491Q        SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK;       // Turn on clock to Port A module        PORTA_PCR13 = PORT_PCR_MUX(1);           // PTA13 is configured as GPIO        GPIOA_PCOR |= 1<<13;                     // Set PTA13 pin low        GPIOA_PDDR |= 1<<13;                     // PTA13 pin is an output                //PIT initialization        SIM_SCGC6 |= SIM_SCGC6_PIT_MASK;         // Turn on clock to to the PIT module        PIT_LDVAL0 = 5240;                       // Timeout period = 500us        PIT_MCR = PIT_MCR_FRZ_MASK;              // Enable clock for PIT, freeze PIT in debug mode        PIT_TCTRL0 = PIT_TCTRL_TIE_MASK |        // Enable PIT interrupt                    PIT_TCTRL_TEN_MASK;          // and PIT                //Enable PIT interrupt on NVIC           NVIC_ICPR |= 1 << ((INT_PIT - 16) % 32);        NVIC_ISER |= 1 << ((INT_PIT - 16) % 32); }   In the PIT interrupt service routine (ISR), there is a variable Counter that is increased by one on every PIT interrupt (500us) and its value is then compared with two preset values. The first preset value EN_HIGH_TIME determines how long the EN pin will remain high to ensure a valid reading of a new set of output data. The second preset value DATA_UPDATE_PERIOD corresponds to the desired output data rate. At the end of the ISR, the PIT interrupt flag is cleared.   void PIT_IRQHandler() {        static int Counter = 0;        Counter++;                                   // Each increment represents 500us        switch (Counter)     {             case 1:             GPIOA_PSOR |= 1<<13;                 // Set EN pin high                      break;             caseEN_HIGH_TIME:                        // 1ms passed             DataReady = 1;                       // Data is ready                      break;             caseDATA_UPDATE_PERIOD:                  // 100ms passed             Counter = 0;                         // Clear Counter at the end of the sample period                      break;             default:                      break;     }        PIT_TFLG0 |= PIT_TFLG_TIF_MASK;              // Clear PIT interrupt flag }   In the main loop, the DataReady variable is periodically checked and if it is set, the accelerometer data registers 0x01 - 0x06 are read and then the acceleration in units of g is calculated. Finally the EN pin is set low to reduce the current consumption and the DataReady variable is cleared.   if (DataReady)                                                                  // Is a new set of data ready? {                  AccData[0] = I2C_ReadRegister(MMA8491Q_I2C_ADDRESS, OUT_X_MSB_REG);         // [7:0] are 8 MSBs of the 14-bit X-axis sample      AccData[1] = I2C_ReadRegister(MMA8491Q_I2C_ADDRESS, OUT_X_LSB_REG);         // [7:2] are the 6 LSB of 14-bit X-axis sample      AccData[2] = I2C_ReadRegister(MMA8491Q_I2C_ADDRESS, OUT_Y_MSB_REG);         // [7:0] are 8 MSBs of the 14-bit Y-axis sample      AccData[3] = I2C_ReadRegister(MMA8491Q_I2C_ADDRESS, OUT_Y_LSB_REG);         // [7:2] are the 6 LSB of 14-bit Y-axis sample      AccData[4] = I2C_ReadRegister(MMA8491Q_I2C_ADDRESS, OUT_Z_MSB_REG);         // [7:0] are 8 MSBs of the 14-bit Z-axis sample      AccData[5] = I2C_ReadRegister(MMA8491Q_I2C_ADDRESS, OUT_Z_LSB_REG);         // [7:2] are the 6 LSB of 14-bit Z-axis sample        Xout_14_bit = ((short) (AccData[0]<<8 | AccData[1])) >> 2;           // Compute 14-bit X-axis output value      Yout_14_bit = ((short) (AccData[2]<<8 | AccData[3])) >> 2;           // Compute 14-bit Y-axis output value      Zout_14_bit = ((short) (AccData[4]<<8 | AccData[5])) >> 2;           // Compute 14-bit Z-axis output value                         Xout_g = ((float) Xout_14_bit) / SENSITIVITY;          // Compute X-axis output value in g's      Yout_g = ((float) Yout_14_bit) / SENSITIVITY;          // Compute Y-axis output value in g's      Zout_g = ((float) Zout_14_bit) / SENSITIVITY;          // Compute Z-axis output value in g's                                              GPIOA_PCOR |= 1<<13;       // Set EN pin low      DataReady = 0;                                                                                                                                 }                       The calculated values can be watched in the "Variables" window on the top right of the Debug perspective or in the FreeMASTER application.       Attached you can find the complete source code written in the CW 10.3 as well as the FreeMASTER project.   If there are any questions regarding this simple application, do not hesitate to ask below. Your feedback or suggestions are also welcome.   Regards, Tomas  
View full article
clicktaleID