Freescale Sensor Fusion Pre-Release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale Sensor Fusion Pre-Release

Freescale Sensor Fusion Pre-Release

The attached is a PRE-RELEASE copy of the next version of the Freescale Sensor Fusion Library for Kinetis MCUs.  It is a pre-release because we are still working to update the datasheet and userguide to accomodate new changes.  The datasheet and user guides included in this copy are identical to the current production versions found at http://www.freescale.com/sensorfusion.  This is the first release of the library which provides ALL SOURCE CODE.  The software license is unchanged from the prior release, and is re-produced at the end of this posting.  Please do not download the file if you can't agree to these license terms.

 

In order to get around virus filter on the community, I've had to create a simple zip file of the fusion toolkit.  There's no installer.  Just unzip it in your directory of choice.

 

Pre-Release Notes for Freescale Sensor Fusion Library for Kinetis MCUs
Previous production release: build 417
This release: build 420

This is a pre-release kit.  The included datasheet and user guide relate to the previous version (build 417).  Updates are in progress and will be published shortly.
In the meantime, changes (at a high level) are listed below.

Changes:
1.  Removed all license checking functions
2.  Fusion and magnetic calibration libraries are now included in source form.    libFusion.a is now gone.  It has been replaced by additional files in the Sources directory. 
3.  Added template projects for Kinetis Design Studio
4.  Added KL46Z board support
5.  Community supported at https://community.freescale.com/community/sensors/sensorfusion
6.  The datasheet has been updated with simulated fusion metrics, code sizes and systick counts
7.  "FLASH_EU" target names have been changed to "FLASH"
8.  Changed branding from "Xtrinsic" to "Freescale".  This resulted in project prefixes  being changed from "XSFK_" to "FSFK_".
9.  Removed the Accelerometer + Magnetometer 6-axis Kalman filter (the eCompass implementation  is more efficient)
10. Debug packets are now on by default.  This enables the Sensor Fusion Toolkit for Android to startup with the correct board display on powerup.
11. The following source files have been renamed:
    FSL_utils.c/.h are now drivers.c/.h
    tasks_func.c/.h are now tasks.c/.h
    proj_config.h is now build.h
    ProcessorExpert.c is now main.c
    baranski_kalman.h is now kalman.h
12. license.h has been removed
13. Added bare metal eCompass implementation for KL46Z (no MQXLite)
14. This version will not include run configurations for all KDS projects. There are too many permutations, and the tools are being regularly updated.

Errata:
1.  Newer K64F Freedom boards can utilize several different versions of the OpenSDA interface.  The MBED drivers do not deal properly with flash security and can temporarily "brick" a board.  In order for the download function to work properly, the value of the NV_FSEC portion of the CPU_FLASH_CONFIG_FIELD within file name Generated_Files/CPU_Config.h must have a value of 0xFE.  Processor Expert (which generates this file) does not currently support that value.  You must make the change manually after running Processor Expert.
2.  When compiling for the first time in KDS, the tool may generate the following error message: "writing to APSR without specifying a bitmask".  This is an invalid error. Simply build a second time and the error will disappear.
3.  MQXLite 1.1.0 created via Processor Expert incorrectly handles contexts switches for the  floating point unit on the K64F.  As shipped, this does not present a problem because  floating point computations are normally completed within one sample period.  However if you add additional code to that project template, such that computations extend beyond one sample period, you will get incorrect results (there is no warning!). MQXLite 1.1.1 fixes this issue.  Check the MQX1 settings in Processor Expert to see which  version you are using.
4.  I2C transmission speeds are configured for 300KHz to 400KHz.   During the build process, it is normal to see the following:
    "Warning: The device is designed to operate up to 100kHz! (SCL frequency)".
    The development team routinely operates at higher I2C frequencies, although these are not necessarily guaranteed in the device datasheets.  Other warnings arise from the  MQXLite code generated by Processor Expert.  The actual fusion library is believed to be clean.

Xtrinsic Sensor Fusion Library for Kinetis MCUs

License: LA_OPT50 Version 20 January 2014

  1. IMPORTANT. Read the following Freescale Software License Agreement (“Agreement”) completely.  By selecting the “I Agree” button at the end of this page, you indicate that you accept the terms of this Agreement and you also acknowledge that you have the authority, on behalf of your company, to bind your company to such terms.  You may then download or install the file.

FREESCALE END-USER SOFTWARE LICENSE AGREEMENT

This is a license agreement between you (either as an individual or as an authorized representative acting on behalf of your employer) and Freescale Semiconductor, Inc. (“Freescale”). It concerns your rights to use software package and any accompanying written materials (the “Software”). The Software includes any updates or error corrections or documentation relating to the Software provided to you by Freescale under this License. In consideration for Freescale allowing you to access the Software, you are agreeing to be bound by the terms of this Agreement. If you do not agree to all of the terms of this Agreement, do not download or install the Software. If you change your mind later, stop using the Software and delete all copies of the Software in your possession or control. Any copies of the Software that you have already distributed, where permitted, and do not destroy will continue to be governed by this Agreement. Your prior use will also continue to be governed by this Agreement.

  1. 1.         LICENSE GRANT. Exclusively in conjunction with Licensee’s development and sale of a product containing Freescale Xtrinsic sensor solutions (e.g., an accelerometer, magnetometer, and a gyroscope in any discrete or combined form factor) supplied directly or indirectly from Freescale (“Freescale System”), or education programs relating to the use of a Freescale System, Freescale grants to you, free of charge, the non-exclusive, non-transferable right (1) to use the Software, (2) to reproduce the Software, (3) to prepare derivative works of the Software, (4) to distribute the Software and derivative works thereof in object (machine-readable) form as part of a Freescale System, and (5) to sublicense to others the right to use the distributed Software as included within the Freescale System. If you violate any of the terms or restrictions of this Agreement, Freescale may immediately terminate this Agreement, and require that you stop using and delete all copies of the Software in your possession or control.   Any license granted above only extends to Freescale’s intellectual property rights that would be necessarily infringed by the Software as provided to you by Freescale and as used within the scope of the licenses granted.  You must advise Freescale of any results obtained including any problems or suggested improvements thereof.  Freescale retains the right to use such results and related information in any manner it deems appropriate.
  2. 2.         OTHER RESTRICTIONS.  Subject to the license grant above, the following restrictions apply:
  3. a.         Freescale reserves all rights not expressly granted herein.
  4. b.         You may not rent, lease, sublicense, lend or encumber the Software, unless otherwise expressly agreed to within this Agreement
  5. c.         You may not distribute, manufacture, have manufactured, sublicense or otherwise reproduce the Software for purposes other than intended in this Agreement.
  6. d.         You may not remove or alter any proprietary legends, notices, or trademarks contained in the Licensed Software,
  7. e.         The terms and conditions of this Agreement will apply to any Software updates, provided to you at Freescale’s discretion, that replace and/or supplement the original Software, unless such update contains a separate license.
  8. f.          You may not translate, reverse engineer, decompile, or disassemble the Software provided to you solely in object code format (machine readable) except to the extent applicable law specifically prohibits such restriction.  You will prohibit your sublicensees from translating, reverse engineering, decompiling, or disassembling the Software except to the extent applicable law specifically prohibits such restriction.
  9. 3.         OPEN SOURCE.  Any open source software included in the Software licensed herein is not licensed under the terms of this Agreement, but is instead licensed under the terms of applicable open source license(s), such as the BSD License, Apache License or the Lesser GNU General Public License.  Your use of such open source software is subject to the terms of each applicable license.  You must agree to the terms of each such applicable license, or you should not use the open source software.
  10. 4.         COPYRIGHT.  The Software is licensed to you, not sold.  Freescale owns the Software, and United States copyright laws and international treaty provisions protect the Software. Therefore, you must treat the Software like any other copyrighted material (e.g. a book or musical recording). You may not use or copy the Software for any other purpose than what is described in this Agreement. Except as expressly provided herein, Freescale does not grant to you any express or implied rights under any Freescale or third party patents, copyrights, trademarks, or trade secrets. Additionally, you must reproduce and apply any copyright or other proprietary rights notices included on or embedded in the Software to any copies made thereof, in whole or in part, if any.  You may not remove any copyright notices of Freescale incorporated in the Software.
  11. 5.         TERM AND TERMINATION.   The term of this Agreement shall commence on the date of installation or download and shall be continue until terminated in accordance with this Agreement. Freescale has the right to terminate this Agreement without notice and require that you stop using and delete all copies of the Software in your possession or control if you violate any of the terms or restrictions of this Agreement.  Freescale may terminate this Agreement should any of the Software become, or in Freescale's reasonable opinion is likely to become, the subject of a claim of intellectual infringement or trade secret misappropriation.  Upon termination, you must cease use of and destroy, the Software and confirm compliance in writing to Freescale. Upon termination, the license granted pursuant to this Agreement immediately terminates and the provisions of Sections 4 through 18 will survive any termination of this Agreement.
  12. 6.         SUPPORT.  Freescale is NOT obligated to provide any support, upgrades or new releases of the Software. If you wish, you may contact Freescale and report problems and provide suggestions regarding the Software. Freescale has no obligation whatsoever to respond in any way to such a problem report or suggestion. Freescale may make changes to the Software at any time, without any obligation to notify or provide updated versions of the Software to you.
  13. 7.         NO WARRANTY.  TO THE MAXIMUM EXTENT PERMITTED BY LAW, FREESCALE EXPRESSLY DISCLAIMS ANY WARRANTY FOR THE SOFTWARE. THE SOFTWARE IS PROVIDED “AS IS”, WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED, INCLUDING, WITHOUT LIMITATION, THE IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, OR NON-INFRINGEMENT. YOU ASSUME THE ENTIRE RISK ARISING OUT OF THE USE OR PERFORMANCE OF THE SOFTWARE, OR ANY SYSTEMS YOU DESIGN USING THE SOFTWARE (IF ANY). NOTHING IN THIS AGREEMENT MAY BE CONSTRUED AS A WARRANTY OR REPRESENTATION BY FREESCALE THAT THE SOFTWARE OR ANY DERIVATIVE WORK DEVELOPED WITH OR INCORPORATING THE SOFTWARE WILL BE FREE FROM INFRINGEMENT OF THE INTELLECTUAL PROPERTY RIGHTS OF THIRD PARTIES.
  14. 8.         INDEMNITY. You agree to fully defend and indemnify Freescale from any and all claims, liabilities, and costs (including reasonable attorney’s fees) related to (1) your use (including your sublicensee’s use, if permitted) of the Software or (2) your violation of the terms and conditions of this Agreement.
  15. 9.         LIMITATION OF LIABILITY.  IN NO EVENT WILL FREESCALE BE LIABLE, WHETHER IN CONTRACT, TORT, OR OTHERWISE, FOR ANY INCIDENTAL, SPECIAL, INDIRECT, CONSEQUENTIAL OR PUNITIVE DAMAGES, INCLUDING, BUT NOT LIMITED TO, DAMAGES FOR ANY LOSS OF USE, LOSS OF TIME, INCONVENIENCE, COMMERCIAL LOSS, OR LOST PROFITS, SAVINGS, OR REVENUES TO THE FULL EXTENT SUCH MAY BE DISCLAIMED BY LAW EVEN IF INFORMED IN ADVANCE OF THE POSSIBILITY OF SUCH DAMAGES.  FREESCALE’S LIABILITY WILL IN ANY EVENT AND UNDER ANY THEORY OF RECOVERY BE LIMITED TO THE TOTAL AMOUNT RECEIVED BY FREESCALE UNDER THIS AGREEMENT.
  16. 10.       COMPLIANCE WITH LAWS; EXPORT RESTRICTIONS. You must not resell, re-export, or provide, directly or indirectly, the licensed software or direct product thereof, in any form without obtaining appropriate export or re-export licenses from the United States Government and from the country from which the export or re-export is to occur.  An export occurs when products, technology, or software is transferred from one country to another by any means, including physical shipments, FTP file transfers, E-mails, faxes, remote server access, conversations, and the like.  An export also occurs when technology or software is transferred to a foreign national in the United States, or foreign national of the country in which the business activity is taking place.  A foreign national is any person who is neither a citizen nor permanent resident of the United States, or the country in which the business activity is taking place. Furthermore, if an export/import license, permit or other government required authority (collectively referred to as “government authorization”) is required to transfer technology, software, hardware or other Freescale property to non- Freescale party(ies) and is not approved, then Freescale is not obligated to transfer the Software under this Agreement until such “government authorization” is granted..
  17. 11.       GOVERNMENT RIGHTS.  The Licensed Software is a “Commercial Item” as defined in 48 C.F.R. §2.101, consisting of “Commercial Computer Software” and “Commercial Computer Software Documentation,” as such terms are used in 48 C.F.R. § 12.212 or 48 C.F.R. §227.7202, as applicable and are only licensed to U.S. Government end users with the rights as are set forth herein..
  18. 12.       HIGH RISK ACTIVITIES.  You acknowledge that the Software is not fault tolerant and is not designed, manufactured or intended by Freescale for incorporation into products intended for use or resale in on-line control equipment in hazardous, dangerous to life or potentially life-threatening environments requiring fail-safe performance, such as in the operation of nuclear facilities, aircraft navigation or communication systems, air traffic control, direct life support machines or weapons systems, in which the failure of products could lead directly to death, personal injury or severe physical or environmental damage (“High Risk Activities”). You specifically represent and warrant that you will not use the Software or any derivative work of the Software for High Risk Activities.
  19. 13.       CHOICE OF LAW; VENUE; LIMITATIONS.  You agree that the statutes and laws of the United States and the State of Texas, USA, without regard to conflicts of laws principles, will apply to all matters relating to this Agreement or the Software, and you agree that any litigation will be subject to the exclusive jurisdiction of the state or federal courts in Texas, USA.  You agree that regardless of any statute or law to the contrary, any claim or cause of action arising out of or related to this Agreement or the Software must be filed within one (1) year after such claim or cause of action arose or be forever barred.
  20. 14.       CONFIDENTIAL INFORMATION.  You must treat the Software as confidential information and you agree to retain the Software in confidence perpetually, with respect to Software in source code form (human readable), or for a period of five (5) years from the date of termination of this Agreement, with respect to all other parts of the Software.  During this period you may not disclose any part of the Software to anyone other than employees who have a need to know of the Software and who have executed written agreements obligating them to protect such Licensed Software to at least the same degree of care as in this Agreement.  You agree to use the same degree of care, but no less than a reasonable degree of care, with the Software as you do with your own confidential information. You may disclose Software to the extent required by a court or under operation of law or order provided that you notify Freescale of such requirement prior to disclosure, which you only disclose information required, and that you allow Freescale the opportunity to object to such court or other legal body requiring such disclosure.
  21. 15.       PRODUCT LABELING.  You are not authorized to use any Freescale trademarks, brand names, or logos.
  22. 16.       ENTIRE AGREEMENT.  This Agreement constitutes the entire agreement between you and Freescale regarding the subject matter of this Agreement, and supersedes all prior communications, negotiations, understandings, agreements or representations, either written or oral, if any.  This Agreement may only be amended in written form, executed by you and Freescale.
  23. 17.       SEVERABILITY.  If any provision of this Agreement is held for any reason to be invalid or unenforceable, then the remaining provisions of this Agreement will be unimpaired and, unless a modification or replacement of the invalid or unenforceable provision is further held to deprive you or Freescale of a material benefit, in which case the Agreement will immediately terminate, the invalid or unenforceable provision will be replaced with a provision that is valid and enforceable and that comes closest to the intention underlying the invalid or unenforceable provision.
  24. 18.       NO WAIVER.  The waiver by Freescale of any breach of any provision of this Agreement will not operate or be construed as a waiver of any other or a subsequent breach of the same or a different provision.

    © 2004-2014 Freescale Semiconductor, Inc. All rights reserved.

Labels (1)
Attachments
Comments

Are there plans for releasing the library for Non-Windows KDS implemetations?

No ratings
Version history
Last update:
‎02-03-2026 05:14 PM
Updated by: