programmable/ erasable ICODE DNA/slix

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

programmable/ erasable ICODE DNA/slix

3,009 Views
vamsikrishna_ta
Contributor II

 

are there any kind of IC/Tags/Boards or simulators which acts as icode Dna(must support ISO 15693) and responds to all commands, what the exact intension is

1) i want to change its uid.

2). i want to erase and rewrite all the blocks even they are locked / read or write protected.

3. a kind of factory reset where it the keys can be reconfigured even they are locked and activate.

 

Tags (4)
0 Kudos
Reply
3 Replies

3,001 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vamsikrishna_ta ,

 

Actually I have no idea of such kind product/IC, but what is the purpose you are looking for this kind of product? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,988 Views
vamsikrishna_ta
Contributor II

hi @Kan_Li ,

we need to use a lot of icode dna tags for testing purposes, in the process we are wasting many tags as once the tag is programmed with key and activated we cannot able to modify the contents on it . so ,our plan is to reduce programming effors and wastage of tags, we are searching out for a solution that acts a icode dna tag that can be erasable although it is locked and protected.

0 Kudos
Reply

2,974 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vamsikrishna_ta ,

 

Thanks for the clarification! Actually UID is permanently set by NXP and is locked(read only), so it is not possible to change it out of factory.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply