about the latest SE05x_MW file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about the latest SE05x_MW file

1,787 Views
tiger_gao
Contributor I

Hi,

     in AN13030 v1.8 version, it metioned the latest se05x recipe (se05x_4.0.0.bb) in the the source code package (SE050-PLUG-TRUST-MW-v04.00.00.zip). but after checked with the package (se05x-PLUG-TRUST_mw_v04.01.01.zip),  the yocto bb is se05x_3.1.0.bb.

      Could anyone provide the latest package to support the latest se05x recipe (se05x_4.0.0.bb) ? thanks!

0 Kudos
Reply
1 Reply

1,774 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @tiger_gao ,

 

Referring to the comments inside, looks like it is a general script which can be used for any version of MW, please kindly refer to the following for details.

Kan_Li_0-1650874645543.pngKan_Li_0-1650874645543.png

 

Please kindly let me know if there is any further issue.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply