SE050: ISO14443 Can support also the B type ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050: ISO14443 Can support also the B type ?

1,958 Views
cant
Contributor II

Dear all, I see that the SE050Cx supports the ISO14443 RFID HF standard, but in the d.s. and other documentation is not clear if it supports also the ISO14443B standard, I see that it supports the Mifare that is an ISO14443A family.

Please clarify in the d.s.

I suppose it supports only the A type.

Thanks a lot

Tags (1)
0 Kudos
Reply
1 Reply

1,843 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, your understanding is correct. NXP cards so far always support only Type A.

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply