SE050: ISO14443 Can support also the B type ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050: ISO14443 Can support also the B type ?

1,950件の閲覧回数
cant
Contributor II

Dear all, I see that the SE050Cx supports the ISO14443 RFID HF standard, but in the d.s. and other documentation is not clear if it supports also the ISO14443B standard, I see that it supports the Mifare that is an ISO14443A family.

Please clarify in the d.s.

I suppose it supports only the A type.

Thanks a lot

タグ(1)
0 件の賞賛
返信
1 返信

1,835件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, your understanding is correct. NXP cards so far always support only Type A.

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信