ReadObject within User Session and VerifySessionUserID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ReadObject within User Session and VerifySessionUserID

2,281件の閲覧回数
priyanka_priyad
Contributor II

Hello,

 

I am using NXP SE050 smartcard with kinetics K64 evaluation board. 

I have tested various commands from NXP APDUSpecifications document. But I am having problem with policies and sessions.

I have created a new User session, and created a binary file in this session with read policies, but when I try to read that file, it is giving the error "command not allowed".

Is there any thing extra that needs to be added in the ReadObject command while trying to read the binary file with read policy?

 

Further, I am not able to verify the session with verifySessionUserID command after creating a new User Session, it gives the error "Conditions not satisfied".

I don't know is there something that I am missing in writing these command APDUs Or there are some additional APDUs that I need to send before sending above mentioned commands or APDUs?

 

Thank you

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,195件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello,

Please don't create multiple threads on the same topic. Thanks for your understanding!

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信