Rasperry Pi/OM-SE050ARD Jumper Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rasperry Pi/OM-SE050ARD Jumper Configuration

1,816 Views
t_buening
Contributor I

Hello,

right now I am trying to connect the OM-SE050ARD board to a Raspberry Pi. But it seems that there is a small error in the documentation (Quick start guide with Raspberry Pi). Which configuration is correct? Is it the left one or the right one?

Regards

Tobias

pastedImage_1.png

0 Kudos
Reply
1 Reply

1,735 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Tobias,

Don't care about J25 & J26, they are dummy jumpers. Please refer to the following for details.

pastedImage_1.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply