Please provide a working SE050 Plug & Trust example for NXP MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Please provide a working SE050 Plug & Trust example for NXP MCU

3,036 Views
Srinivas_M
Contributor I

Hello NXP Team,

I am working on integrating the SE050 secure element with an NXP microcontroller S32K144 using the Plug & Trust middleware. I have reviewed the Plug & Trust SDK and its demos, but I am looking for:

A complete, working example project for any NXP MCU that:

  • Initializes I²C and communicates with SE050
  • Demonstrates setup and a basic operation.
  • Runs on bare-metal or FreeRTOS

Could you please share:

  • A reference project or demo that compiles and runs on a specific NXP board?

Thankyou.

 

 

0 Kudos
Reply
3 Replies

3,011 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Srinivas_M ,

 

Can you accept zephyr instead? The nano package can be integrated with any platform supported by zephyr, such as s32k148evb.  https://github.com/zephyrproject-rtos/zephyr/tree/main/boards/nxp/s32k148_evb  

 

Please kindly refer to https://github.com/NXPPlugNTrust/nano-package/blob/master/zephyr/readme.rst for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,005 Views
Srinivas_M
Contributor I

@Kan_Li, It means For S32K144 also we need to integrate to zephyr OS.?

Mandatorily OS is needed.? On Baremetal S32K144 Can't we integrate Plug and Trust Middleware.?

0 Kudos
Reply

2,970 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Srinivas_M ,

 

Integration based on Zephyr is a quick solution for your case, while porting to S32K144 on Baremetal is technically possible, but no ready solution yet, you have to do it by yourself according to https://github.com/NXPPlugNTrust/nano-package/tree/master?tab=readme-ov-file#porting . 

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply