PN7462AU Example project on PN7412

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462AU Example project on PN7412

ソリューションへジャンプ
5,995件の閲覧回数
Vlatakomarac
Contributor II

Hello,

I want to use PN7412 in my design for contact smart card project.

But I will need to program it with an example software that is provided as a link from UM10883.

Can PN7412 be programmed by examples that are meant for PN7462?

Thank you in advance!

0 件の賞賛
返信
1 解決策
5,867件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

There is no library for PN7412, customers can modify it by themselves.

Regards

Daniel

 

元の投稿で解決策を見る

7 返答(返信)
5,855件の閲覧回数
Vlatakomarac
Contributor II

Hello @danielchen

Now all I need to know is, do I need to change the PN7462 example project to program my PN7412? Or can I just program the PN7412 with the available code for PN7462, would that work? I am guessing it won't work without any changes but I have to make sure with you.

And in the case that I do need to change the code. What exactly do I need to change? Is it enough to just delete all code related to contactless functionalities and leave contact functionalities entact?

 

Thank you! Regards,

Vulinovic Nikola

0 件の賞賛
返信
5,990件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Vlatakomarac :

 

Yes, PN7462 can programmed with an example software.

In UM10883, you can see  how to Import/Build/Run/Debug provided SW example projects .please refer to section 8.5~section 8.7 for more details.

danielchen_0-1640833416773.png

 

 

Regards

Daniel

 

 

 

0 件の賞賛
返信
5,980件の閲覧回数
Vlatakomarac
Contributor II

Hello @danielchen

Thank you for your answer. But I want to know can PN7412 be programmed by the same software examples or are there some examples especially for this IC?

When I look at the PN7462 family, I am interested in PN7412 and not in PN7462. I just need contact card application without contactless card functionalities.

Untitled.png

Thank you! Best regards.

0 件の賞賛
返信
5,972件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Vlatakomarac :

 

We can easily modify existing PN7462 examples to keep the CT interface only. Then we have a FW fit for PN7412.

So we will eliminate CL task and clean up the source.

 

Regards

Daniel

0 件の賞賛
返信
5,910件の閲覧回数
Vlatakomarac
Contributor II

Hi @danielchen 

I have found PN7462 example source code. So do you mean that I should change the source code to remove the contactless functionalities and keep the contact card funcionalities? 

You said in your reply "So we will eliminate CL task and clean up the source."

Does this mean that NXP will offer this new code for PN7412 on its website maybe for download?

Please correct me if I misunderstood. Thank you again for your replies.

Regards

Vulinovic Nikola

0 件の賞賛
返信
5,868件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

There is no library for PN7412, customers can modify it by themselves.

Regards

Daniel

 

5,859件の閲覧回数
Vlatakomarac
Contributor II

Thank you @danielchen !

That is what I wanted to know!

Best regards,

Vulinovic Nikola

0 件の賞賛
返信