Failure in Se05x_API_SessionOpen on SE052F (Raspberry Pi I2C Communication Issue)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure in Se05x_API_SessionOpen on SE052F (Raspberry Pi I2C Communication Issue)

11,501 Views
krsuresh
Contributor III

Hi Team,

I am facing an issue while trying to communicate with the SE052F over I2C using the Plug & Trust Nano Package.
According to the AN14277 application note, I configured the SCP03 keys as follows:

ENC Key: 3ae441c747e32ebc16b3bb2d843c6dd8
MAC Key: 6c18f3d08fee1cb96a3c8de5d3538aaa

However, Se05x_API_SessionOpen consistently fails.

System Information
Platform: Raspberry Pi
Package: Plug and Trust Nano Package v1.5.4
Example used: ex_se05x_GetInfo

 

Log Details:

./ex_se05x_GetInfo
Se05x Getinfo Example !
Plug and Trust nano package - version: 1.5.4
I2C driver supports plain i2c-level commands.
APDU Tx> :00 a4 04 00 0b d2 76 00 00 85 30 4a 43 4f 90 03 00
Failed writing data (nrWritten=-1).
Se05x_API_SessionOpen failedError in Se05x_API_SessionOpen
SE05x Getinfo Example Failed !

I2C Detect details in Raspberry Pi:
flexxon@raspberrypi:~/SE050/NEW-NANO/se052f/nano-package/examples/se05x_GetInfo/linux/build $ i2cdetect -y 1
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- 48 -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

 

Thanks,

Sureshkumar R

Labels (1)
0 Kudos
Reply
23 Replies

511 Views
Ben-FLX
Contributor I

@Kan_Li I am assuming that the MW will be further delayLast update was 6 months ago based on 31/3/2026 10.16am (+8GMT timestamp)Last update was 6 months ago based on 31/3/2026 10.16am (+8GMT timestamp)ed?

 

0 Kudos
Reply

667 Views
Ben-FLX
Contributor I

@Kan_Li 

 

Thanks for the update on the new outlook. Is there anyway that we can get NXP's commit on this new outlook and not merely just a mirage that will not materialize when end March comes?

 

I don't know of any other means to voice this distasteful aftertaste apart from swallowing this  news as is and knowing that we cannot make progress on SE052.

Perhaps, we should seriously consider other vendor...

0 Kudos
Reply

648 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Ben-FLX ,

 

GitHub nano-Pkg is now updated, But It is not yet a release, It is a pre-release ,you may simply git clone it for evaluation purpose. The Release process will be completed along with the Main Package release tentatively planned for 31st March 2026. 

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply