EdgeLock SE050 for PX4 firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EdgeLock SE050 for PX4 firmware

Jump to solution
578 Views
parags
Contributor I

Dear community,

We are currently implementing secure element based security for our PX4-based drone firmware. The pixhawk hardware supports SE050 + Kinetis K66_180 MPU. We have already explored the SE050 EVK board + RPi configuration and are able to store the keys in the secure element in the SE050 EVK  setup. However, we are not successful in integration of SSS APIs into PX4 yet and unsure if this is a right approach.  

Does anybody have any experience with the PX4 + SE050 integration and have any pointers? It would be greatly helpful.

Thank you for your support. 

Regards,

ParagS

 

 

0 Kudos
Reply
1 Solution
569 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @parags ,

 

As far as I know, the MW supports Kinetis K64 FRDM platform, so it should be much easier to port it to K66. The SDK based MW can be downloaded from https://www.nxp.com/webapp/Download?colCode=SDK-EVK-FRDMK64F-SE05X&appType=license .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
570 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @parags ,

 

As far as I know, the MW supports Kinetis K64 FRDM platform, so it should be much easier to port it to K66. The SDK based MW can be downloaded from https://www.nxp.com/webapp/Download?colCode=SDK-EVK-FRDMK64F-SE05X&appType=license .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply