S32K3 Functional Safety Mechanism Consultation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Functional Safety Mechanism Consultation

886件の閲覧回数
Yongxingjia
Contributor II

S32K3 is designed with a lot of functional safety mechanisms, but in the actual product, there may be limited related functions that cannot be used, for example:

1.the ECU only uses SPI0 and does not use other SPI controllers, so do other SPI controllers need to be checked for SAF at this time?

2.If I don't use a CAN controller, do I need to check the CAN controller?

3.If you do not perform safety checks on unused peripheral resources, will the functions of the used peripheral resources be affected?

0 件の賞賛
返信
0 返答(返信)