Hi
We have talked about questions of working altitude. And the discussion is marked as solved. As below:
Our product may working in altitude upto 4800m.
Pls help to provide the failure rate or FMEDA in this condition. (Considering that altitude>2000m,the soft-error rate shall be increased by a appropriate factor according to e.g. JESD89A.)
Thanks
Hi Aarul
Thanks for answer.
Our project is in certification process by TUV.
They have two concern:
1. How does NXP get the factor(15.147 on 4800m)? Is it based on any standard(which standard)?
2. Why Flash doesn't need to consider transient failures? TUV think the "soft error" will increase anyhow in high altitude. what's the robust design of S32K144?
Need your help!
Thank you!
1. The failure rates at sea-level are based on measurements performed in compliance with JESD89A. The scaling factor for the neutron flux is calculated at http://www.seutest.com/cgi-bin/FluxCalculator.cgi. JESD89A refers to this link for the neutron flux calculation.
2. To my best knowledge, flash bit cells are not sensitive to soft-error due to technology (low density planar embedded NVM ) used by NXP. During testing state change of bit cells was not observed. Please also note that irrespective of this we do have ECC correction logic on Flash which can correct any error at higher altitudes. So there shouldn't be any safety issues to assessor.
Regards
-Aarul