S32G IPCF functional safety assumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G IPCF functional safety assumption

ソリューションへジャンプ
793件の閲覧回数
zeyu_yan
Contributor III

Hello,

      I use S32G IPCF to trasnfer signal from Mcore to Acore, and what is the assumption for IPCF to achieve ASIL B, should we create a protocol including E2E (CRC,Counter,Data ID)?

0 件の賞賛
1 解決策
788件の閲覧回数
nxa11829
NXP Employee
NXP Employee

Hi,

 

If the memory used for data sharing between cores is ECC protected then E2E is not required. IPCF software is developed to ISO26262. Required assumptions are documented in the IPCF safety manual. This will be available in the RTM release at end of January 2022, when SafetyPackage_IPCF_*zip will be published in flexera.

 

Many thanks,

Alison

元の投稿で解決策を見る

0 件の賞賛
5 返答(返信)
789件の閲覧回数
nxa11829
NXP Employee
NXP Employee

Hi,

 

If the memory used for data sharing between cores is ECC protected then E2E is not required. IPCF software is developed to ISO26262. Required assumptions are documented in the IPCF safety manual. This will be available in the RTM release at end of January 2022, when SafetyPackage_IPCF_*zip will be published in flexera.

 

Many thanks,

Alison

0 件の賞賛
771件の閲覧回数
zeyu_yan
Contributor III

hello,I still can not find this zip, where should I download this file(SafetyPackage_IPCF_*zip)?

thank you.

0 件の賞賛
764件の閲覧回数
naveenm
NXP Employee
NXP Employee

Hi,

I am waiting for an answer from appropriate team to provide me the location of SafetyPackage_IPCF_*zip.

Will get back to you as soon as I receive reply.

 

Thanks for your patience.

Regards,

NaveenM

 

0 件の賞賛
783件の閲覧回数
zeyu_yan
Contributor III

Great,,thank you!

where should I download this safety manual when it is released?

タグ(1)
0 件の賞賛
791件の閲覧回数
zeyu_yan
Contributor III

hello , I want to know , if I only apply <Memory protection> , can I achieve ASIL B or D? or there are other assumption ? like Safety mechanism E2E?

zeyu_yan_0-1641816953788.png

 

0 件の賞賛